cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-AZRTOS-H7 V2.0.0 compatibility with STM32CubeMX 6.5.0

Asantos
Senior

I installed the just released STM32CubeMX 6.5.0 and noted that the X-CUBE-AZRTOS-H7 V2.0.0 is not compatible with it. Is there some setting to correct it or do I need to wait for the new release of the AZRTOS?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @Community member​ ,

Please refer to the answer provided by Chekib regarding your same request in this discussion.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.