2020-04-17 3:04 AM
There is a wrong comment in AN2606 (Rev 42) in Table 130 for STM32L552 and CAN Bootloader
The Comment for FDCAN bootloader tells:
USB FS configured in forced device
mode.
USB FS interrupt vector is enabled and
used for USB DFU communications.
Note: VDDUSB IO must be connected to
3.3V for USB to be operational.
I assume that this is however the comment related to DFU bootloader.
Instead there should be a definition for the CAN Bitrate (as in all the other comments for CAN bootloader) like this:
Once initialized the CAN1 configuration
is:
Baudrate 125 kbps, 11 -bit identifier.
I assume the CAN Bootloader for teh STM32L552 is using the same configuration as this is what we want to use together with STLINK-V3Set now.
Any confirmation appreciated.
2020-04-17 3:32 AM
Hi GS@S,
Thank you so much for your feedback.
Yes we confirm that.
This will be updated very soon.
Best Regards,
Ons.