Writing to external Flash through QSPI using an STM32L4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-04-25 9:32 PM
Hello all,
I am working with a board that features an STM32L4 and I would appreciate some pointers on writing and reading to the external flash. The device I am using is the MX25R6435F and I have been able to read the device ID without any problem with the following code.
#define RDID 0x9F
QSPI_HandleTypeDef hqspi;
QSPI_CommandTypeDef sCommand;
uint8_t reg[3];
sCommand.InstructionMode=QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction=RDID;
sCommand.AddressMode=QSPI_ADDRESS_NONE;
sCommand.AlternateByteMode=QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode=QSPI_DATA_1_LINE;
sCommand.DummyCycles=0;
sCommand.Address=0;
sCommand.DdrMode=QSPI_DDR_MODE_DISABLE;
sCommand.SIOOMode=QSPI_SIOO_INST_EVERY_CMD;
sCommand.NbData=3;
HAL_QSPI_Command(&hqspi, sCommand, 1000)
HAL_QSSPI_Receive(&hqspi, reg, 1000);
However, problems arise when I try to modify the above code to write values to the device.
The MX25R64's datasheet mentions PP, Page Program, and WREN, Write Enable. I initially set both instructions and then tried to transmit and receive data, but I did not read the right value back from the flash.
#define WREN 0x06
#define PP 0x02
sCommand.InstructionMode=QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction=WREN;
sCommand.AddressMode=QSPI_ADDRESS_NONE;
sCommand.AlternateByteMode=QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode=QSPI_DATA_1_LINE;
sCommand.DummyCycles=0;
sCommand.Address==Addr;
sCommand.DdrMode=QSPI_DDR_MODE_DISABLE;
sCommand.SIOOMode=QSPI_SIOO_INST_EVERY_CMD;
sCommand.NbData=3;
sCommand.InstructionMode=QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction=PP;
sCommand.AddressMode=QSPI_ADDRESS_NONE;
sCommand.AlternateByteMode=QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode=QSPI_DATA_1_LINE;
sCommand.DummyCycles=0;
sCommand.Address=Addr;
sCommand.DdrMode=QSPI_DDR_MODE_DISABLE;
sCommand.SIOOMode=QSPI_SIOO_INST_EVERY_CMD;
sCommand.NbData=3;
I am confused about where to proceed from here because I'm not sure if following the above code with HAL_QSPI TX and RX commands is enough
HAL_QSPI_Transmit(&hqspi, pData, Timeout);
HAL_QSPI_Receive(&hqspi, pData, Timeout);
I was wondering if anyone had any insight into writing to this device. I am new to QSPI so I'm not sure if my problems are related to my misinterpretation of the datasheet or the interface.
- Labels:
-
QSPI
-
STM32Cube MCU Packages
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-04-25 9:45 PM
Review BSP code examples for assorted DISCO and EVAL series boards.
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
‎2019-04-25 11:04 PM
Hello Clive,
I actually have been able to work with the QUADSPI Flash on a B-L475e-iot01a board. I started to move away from the BSP_QSPI functions because I had trouble envisioning how I would integrate the BSP files into a custom build. I just found this link for integrating BSP files into a project so I'll check it out. Is there any other recommended approach for integrating BSP files into builds?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-04-26 5:53 PM
I actually looked into the BSP programs in depth and I can see the code behind the BSP abstraction. I don't know how I missed it before but I can just emulate those
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-04-26 6:17 PM
ST layers and abstracts things a lot, arguably too much, but in a way that's convenient to them across many boards/families.
I'm reasonably comfortable just using the HAL layer, and taking the pieces I need and making a more concise linear implementation. When I want things functional earlier, ie pre-main() or C runtime/startup, I'll build something cleaner I can put in SystemInit() at a register level (no external dependencies) or assembler in Reset_Handler.
Up vote any posts that you find helpful, it shows what's working..