2017-12-06 1:13 AM
Hello,
I used the STM32L073RZ and I used Stop mode for saving current.
And my problem is when I measured the current consumption of this MCU, I found arround 3uA during only 3 minutes after starting the Stop mode and then arround 15uA until my system wake-up, as you can see on the next chart the Current consumption measure with X-NUCLEO-LPM01A at the
increase of current
:I already check the same result with an amperemeter.
It is like some internal power supply just turn on, but my system is always in stop mode.
I put the MCU in stop mode with the HAL driver function like that:
/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE();/* Enable Ultra low power mode */
HAL_PWREx_EnableUltraLowPower();/* Enable the fast wake up from Ultra low power mode */
HAL_PWREx_EnableFastWakeUp(); HAL_SuspendTick(); //Request to enter STOP mode with regulator in low power mode HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); HAL_ResumeTick();//After wake-up from STOP reconfigure the PLL SystemClock_Config();Where :
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit;/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE(); /* The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency, to update the voltage scaling value regarding system frequency refer to product datasheet. */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); /* Disable Power Control clock */ __HAL_RCC_PWR_CLK_DISABLE(); /**Initializes the CPU, AHB and APB busses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.LSIState = RCC_LSI_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4; RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_4;if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{ Error_Handler(); } /**Initializes the CPU, AHB and APB busses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{ Error_Handler(); }PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_LPUART1
|RCC_PERIPHCLK_I2C1|RCC_PERIPHCLK_I2C3 |RCC_PERIPHCLK_RTC; PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1; PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1; PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1; PeriphClkInit.I2c3ClockSelection = RCC_I2C3CLKSOURCE_PCLK1;PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{ Error_Handler(); }//Configure the Systick interrupt time
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); //Configure the Systick HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK); //SysTick_IRQn interrupt configuration HAL_NVIC_SetPriority(SysTick_IRQn, 3, 0);}And just before Put the system in stop mode, I cut all interfaces that I don't need except one UART and 6 IO.
I don't that the problem come from the interface that I let awake because as I said, the
increase of current
is during the stop mode.According to you, where could this increase of current come from during the stop mode?
#stm32-l0 #stop-mode #hal-pwr2017-12-07 11:49 AM
I can't believe that such an oscillation (very nice capture!) may come from anywhere else than the external environment of the MCU.
Concerning the consumption, I bet that the MCU is somehow activated (from the outside) but is internally configured not to wake on that event. I/O configuration is likely to be the clue of this issue. How is it done ? Can you close all I/O and see how behaves the current ?
2017-12-08 5:47 AM
Oh, thank you,
I never thought that the MCU could be have this behaviour (activated by something not configure for)
I will try it.
2017-12-08 6:58 AM
Well I cut each IO of the MCU and I have always the problem.
Also, I try the same test with an other board with the same components and I don't have the problem.
So perhaps I damaged my MCU by soldering or with static electricity.
In all cases, the
X-NUCLEO-LPM01A is really great to current measurement.
2017-12-08 9:59 AM
Floating inputs can make current consumption to vary randomly. Does the current change if you move your hand close above the board. Floating inputs can do that too.
2018-02-01 5:46 AM
Normally, I initialized all non used pinout as analog. Perhaps I missed some of them.
2023-08-30 5:31 AM