2023-07-29 11:50 AM
In the Application Note for the ST Bootloader, DFU bootloader commands such as DFU_DNLOAD are specified. Where would I, as a programmer, use these commands? When communicating with the STM32 microcontroller using the ST Programmer via the command line, I have different commands. Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?
Solved! Go to Solution.
2023-07-29 11:59 AM
> Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?
Of course it is.
2023-07-29 11:59 AM
> Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?
Of course it is.