Update STM32F767zi firmware through system bootloader via USB-stick
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-28 2:58 PM
Hi,
I saw that it is possible to flash firmware via the Cube Programmer and the System Bootloader. Is it also possible to update the device through the system bootloader from a USB stick?
Also, does someone have a suggestion where I can find more information about the build- in bootloader other than the application note?
Thank you very much
Solved! Go to Solution.
- Labels:
-
STM32Cube MCU Packages
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-28 3:16 PM
No it doesn't support such a mode.
There's a FW Upgrade / IAP example for several F4 and F7 boards using the USB MSC HOST and FatFs. Similarly you could create something to use a MicroSD card, or Ethernet.
The ISP has very finite modes of operation, not all eventualities on all boards.. Use AN2606 as controlling..
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
‎2023-07-28 3:16 PM
No it doesn't support such a mode.
There's a FW Upgrade / IAP example for several F4 and F7 boards using the USB MSC HOST and FatFs. Similarly you could create something to use a MicroSD card, or Ethernet.
The ISP has very finite modes of operation, not all eventualities on all boards.. Use AN2606 as controlling..
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
‎2023-07-28 10:55 PM
Ok thank you, now I have clarity. Thank you very much for your answer