cancel
Showing results for 
Search instead for 
Did you mean: 

Using with LwIP stuck the task

Lmali.1
Associate III

Hello,

​I download a file from server with netcomm_recv.

​l write in FreeRTOS, with several tasks.

For this discussion, l have two tasks.

One is general task and the other​ is for downloading the file from server.

From the first task, there is a condition that send a queue message to the second task to start download.

If both tasks are in the same ​priority, the downloading task doesn't run.

It l set the downloading task with higher priority, this task works perfectly, but the first task doesn't run.

For reference, the first task blink a LED.

once the first task stuck (in the second case), the LED is stay on the same position (doesn't blink).

What do I do wrong?

What am l missing?

Thanks,

Lior​

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Piranha
Chief II