Skip to main content
Manny
Associate II
January 6, 2022
Question

Using the Freertos CORTEX_M4F_STM32F407ZG-SK with stm32f401cc (black pill v2).

  • January 6, 2022
  • 1 reply
  • 935 views

Hello,

I wanted to use the CORTEX_M4F_STM32F407ZG-SK demo of free rtos with stm32f401cc. In the past I have used this demo with stm32f405rg, I have changed the PLL setting for 84Mhz as:

// in stm32f4xx.h

#define HSE_VALUE  ((uint32_t)25000000)

// in system_stm32fxx.c

/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */

#define PLL_M   25

#define PLL_N   336

/* SYSCLK = PLL_VCO / PLL_P */

#define PLL_P   4

/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */

#define PLL_Q   7

I am using IAR(and changed the mcu to stm32f401cc), but when I run the code, it jumps directly to the HardFault_Handler without going through main. I am using FreeRTOSv202104.00 version.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
January 6, 2022

Check SystemInit() code.

Make sure it enables FPU.

Look at what instructions fault, the CPU has registers.

Use the debugger to step in from Reset_Handler, it unchecked "run to main()" type options.

Check initial stack pointer is within RAM of MCU​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..