2020-12-14 10:03 PM
Hello, i want to use USB FS with f303re.
last time, i used USB CDC FS with my f303ze,
use function of 'CDC_Transmit_FS', so i can see text in computer with terminal program.
i saw that f303re have USB FS in cubeMX, but i think f303re can't use CDC_Transmit_FS.
then how can i communication between nucleo - f303re and computer?
if f303re can't communication with computer, What is the purpose of USB FS ?
2020-12-22 02:01 AM
Hi Jlee.8,
In fact, the difference between these two boards is that the Nucleo_F303RE is a 64 pins board and Nucleo_F303ZE is a 144 pîns board. Therefore, STM32F303RE is missing the USB connector however it does support USB FS features including CDC. So, you can use all functions related including the "CDC_Transmit_FS" one.
In order to use the USB of the Nucleo-F303RE board, you have to use a USB shield or costum configuration by setting the suitable connection of D+, D-, Vbus, and GND.
I hope my answer is helpful.
Best Regards,
Ons.