Skip to main content
Senior
October 13, 2024
Solved

STM32F303 does not boot

  • October 13, 2024
  • 2 replies
  • 1013 views

Hi,

I run the NUCLEO-F303RE eval board. I separated the ST-Link part from the target processor part and connected GND/TCK/TMS/NRST/SWO by wires. I populated the 8MHz xtal with Rs and Cs on the target part. 

This works fine.

I copied the circuitry for the target processor according to UM1724 documentation for my own board with populated xtal. I connected it to the ST-Link and flashed it with CubeIDE.

I read "Verifying ....." and "Download verified successfully" . So flashing seems to work.

Then I constantly get: "Target is not responding, retrying" 

The xtal is not oscillating. The target processor does nort work either with direct MCO clock from ST-Link.

I checked Vdd and GND. I checked BOOT0 pin 10k to GND. VDDA and VBAT is not applied. 

What does it need more to start?

THX Cheers

Detlef

This topic has been closed for replies.
Best answer by Tesla DeLorean

VDDA/VSSA is required. It's not just if you use ADC/DAC, but it also runs the PLL and POR circuits.

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
October 13, 2024

VDDA/VSSA is required. It's not just if you use ADC/DAC, but it also runs the PLL and POR circuits.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DetlefSAuthor
Senior
October 13, 2024

:) . Yes, was not aware of that. Bought you a coffee or a beer.

Cheers

Thanks

Detlef