2016-05-29 11:30 PM
I have emulated two VCPs with only one USB Device. I can send data in one VCP that has the following Endpoint Address.
#define CDC_IN_EP 0x81 /* EP1 for data IN */#define CDC_OUT_EP 0x01 /* EP1 for data OUT */#define CDC_CMD_EP 0x82 /* EP2 for CDC commands */
I would like to know if it's possible to send data in the other VCP with other Endpoint Address like :
#define CDC_IN_EP3 0x83 /* EP3 for data IN */#define CDC_OUT_EP3 0x03 /* EP3 for data OUT */#define CDC_CMD_EP4 0x84 /* EP4 for CDC commands */
My problem is that addresses others than 0x81 don't allow me to send data over the second VCP. I'm using two CDC interfaces Full-Speed. Normally we can use 7 endpoints with CDC_FS and that's what I'm trying to do.. I have 6 Endpoints: 3 for each VCP and the seventh is Endpoint 0 for configuration.
Have I missed something in the Endpoints Configuration or in the Composite Device Descriptors ?
Thank you guys.
#usb #stm32 #usb #cdc #cdc #vcp #endpoints2016-05-30 7:28 AM
Hi el_alaoui.moulay_has,
USB CDC spec allow no more than one IN endpoint at single Communication Data class interface. Refer to this for more information -Hannibal-2016-05-30 11:48 PM