2020-09-16 12:17 AM
Hi Stmteam,
I am using Stm32G081RB to Develop Source application.
please have a look at the source files and trace.
Note : trace file is from sink device attached to the Source Device currently we are looking to Develop complete solution.
Questions:
Note : ADC reading after the power establishment is proper. I make sure the voltage read by the USBPD stack is correct by putting break point at BSP_PWR_VBUSGetVoltage in usbpd_pwr_user.c file.
Kindly don't hesitate to revert back (at any time) for more information about the product.
Thanks and Regards
Himavanth
2020-09-29 4:47 AM
Hi Yohann M,
After a lot of hours spending on debugging through the application, I found USBPD_PWR_IF_SetProfile function returning USBPD_OK, and responds time also so quick.
Note :
after the execution of USBPD_PWR_IF_SetProfile function control is transferred to piece of code attached below:
osEvent osMessageGet (osMessageQId queue_id, uint32_t millisec)
{
portBASE_TYPE taskWoken;
TickType_t ticks;
osEvent event;
event.def.message_id = queue_id;
event.value.v = 0;
if (queue_id == NULL) {
event.status = osErrorParameter;
return event;
}
taskWoken = pdFALSE;
ticks = 0;
if (millisec == osWaitForever) {
ticks = portMAX_DELAY;
}
else if (millisec != 0) {
ticks = millisec / portTICK_PERIOD_MS;
if (ticks == 0) {
ticks = 1;
}
}
if (inHandlerMode()) {
if (xQueueReceiveFromISR(queue_id, &event.value.v, &taskWoken) == pdTRUE) {
/* We have mail */
event.status = osEventMessage;
}
else {
event.status = osOK;
}
portEND_SWITCHING_ISR(taskWoken);
}
else {
if (xQueueReceive(queue_id, &event.value.v, ticks) == pdTRUE) {
/* We have mail */
event.status = osEventMessage;
}
else {
event.status = (ticks == 0) ? osOK : osEventTimeout;
}
}
return event;
}
finally, it's returns with osEventTimeout by the statement in the piece of code attached above.
event.status = (ticks == 0) ? osOK : osEventTimeout;
Thanks & Regards
-Himavanth
2020-09-29 5:19 AM
Hi
PS_RDY is managed internally in the stack. It is described in the above MSC I attached in this thread, sent after calling the function 'USBPD_DPM_SetupNewPower/USBPD_PE_RequestSetupNewPower'.
case PE_SRC_TRANSITION_SUPPLY:
{
if (IS_TIMER_EXPIRED(_pdhandle, PE_GenericTimer))
{
PE_SetPowerNegotiation(_pdhandle, USBPD_POWER_TRANSITION);
/* Request DPM to transition power supply */
/* Setup the new power level */
if (_pdhandle->PE_Callbacks->USBPD_PE_RequestSetupNewPower != NULL)
{
__DEBUG_CALLBACK(_pdhandle, "USBPD_PE_RequestSetupNewPower");
if (USBPD_OK != _pdhandle->PE_Callbacks->USBPD_PE_RequestSetupNewPower(_pdhandle->PE_CurrentPortNumber))
{
SWITCH_TO_STATE_NOTIMEOUT(_pdhandle, PE_STATE_HARD_RESET);
}
else
{
SWITCH_TO_STATE(_pdhandle, PE_SRC_TRANSITION_SUPPLY_EXIT);
}
}
}
break;
}
case PE_SRC_TRANSITION_SUPPLY_EXIT :
{
if (USBPD_OK == PE_Send_CtrlMessage(_pdhandle, USBPD_SOPTYPE_SOP, USBPD_CONTROLMSG_PS_RDY, PE_STATE_READY, USBPD_CA_NONE))
{
PE_SetPowerNegotiation(_pdhandle, USBPD_POWER_EXPLICITCONTRACT);
NOTIFY_EVENT_TO_DPM(_pdhandle, USBPD_NOTIFY_POWER_EXPLICIT_CONTRACT);
#if defined(USBPD_REV30_SUPPORT) && defined(USBPDCORE_PPS)
_pdhandle->PE_ZIVal.PE_Timers.PE_PPSPeriodicTimer = 0u;
/* Start tPPSTimeout timer if APDO has been selected and not running */
if (USBPD_CORE_PDO_TYPE_APDO == _pdhandle->PE_ZIVal.PE_Flags.Flag.PE_CurrentPowerObject)
{
START_TIMER_PE(_pdhandle, PE_PPSPeriodicTimer, PE_TPPSTIMEOUT);
}
#endif /* USBPD_REV30_SUPPORT && USBPDCORE_PPS*/
}
break;
}
I am sorry but I cannot help you more without a USB-PD trace from our stack. You just need to connect a UART TX pin to a ST-Link for instance (RX PIN on CN3 of Nucleo board).
Regards,
Yohann
2020-09-29 6:12 AM
Hi Yohan,
As I am using MB1136 board for SWD programming,
Thanks & Regards
2020-09-29 6:26 AM
Hi
Yes, you can use this board.
On your cubemx application, you can enable TRACER_EMB as described in the "5.2.2 Activation of embedded tracer for debug".
Then, you have to select a UART TX pin and this pin can be connected to your MB1136 board (RX pin on CN3 connector).
Then with CubeMonitor, you should be able to get the traces (as you did for Disco board).
Yohann
2020-10-12 8:05 AM
2020-10-12 11:26 PM
Hi @HGorl.1
Nice to see that now you are able to get the trace.
It seems that PE does not have time to send the PS_RDY. There is CC detach during the power transition after 12ms !?
1796 PE 25877 1 PE_SRC_SEND_CAPABILITIES
1797 OUT 25879 1 SRC_CAPABILITIES DATA:2C9101222CD102002CB104003C2176C0 / 5V - 3A / 9V - 3A / 15V - 3A / [3.3V - 5.9V] - 3A SOP PD3 H:0x41A1
1798 IN 25880 1 GOODCRC SOP H:0x0001
1799 NOTIF 25880 1 SRCCAP_SENT
1800 PE 25880 1 PE_SRC_WAIT_REQUEST
1801 IN 25882 1 REQUEST DATA: 96580231 / ObjectPosition:3 / GiveBack:0 / CapabilityMismatch:0 / USBCommunicationCapable:0 / NoUSBSuspend:1 / UnchunkedExtendedMessagesSupported:0 SOP PD3 H:0x1082
1802 OUT 25882 1 GOODCRC SOP H:0x0121
1803 PE 25883 1 PE_SRC_NEGOTIATE_CAPABILITY
1804 OUT 25883 1 ACCEPT SOP PD3 H:0x03A3
1805 IN 25884 1 GOODCRC SOP H:0x0201
1806 NOTIF 25884 1 REQUEST_ACCEPTED
1807 PE 25884 1 PE_SRC_TRANSITION_SUPPLY
1808 EVENT 25896 1 EVENT_DETACHED
Do you have a protection on your CC lines which can disconnect them?
Did you try at least to get a contract at 5V only? To do it, you could expose only the 1st PD0 in your source capabilities!
Regards,
Yohann
2020-10-13 2:22 AM
One more point... you use an old version of our stack... Can you try to adapt your applications with latest stack I delivered with the ZIP file (USBPD _provider_port1_ST.7z) I sent to you on 25th of September?