2017-02-25 10:10 PM
Hi Everyone,
I'm trying to read from the USB keyboard with a custom board STM32F205RCT6 MCU.
I am using USB FS host (host only) with HAL library.but it just works with some keyboards!
Other keyboards are detected by host but can not read data.
Can any one help me?My Code:
int main(void) { /* STM32F4xx HAL library initialization: - Configure the Flash prefetch, instruction and Data caches - Configure the Systick to generate an interrupt each 1 msec - Set NVIC Group Priority to 4 - Global MSP (MCU Support Package) initialization */ HAL_Init(); /* Configure the system clock to 120 MHz */ SystemClock_Config(); /* Init Host Library */ USBH_Init(&hUSBHost, USBH_UserProcess, 0); /* Add Supported Class */ USBH_RegisterClass(&hUSBHost, USBH_HID_CLASS); /* Start Host Process */ USBH_Start(&hUSBHost); /* Run Application (Blocking mode) */ while (1) { /* USB Host Background task */ USBH_Process(&hUSBHost); if(USBH_HID_GetDeviceType(&hUSBHost) == HID_KEYBOARD) { hid_demo.keyboard_state = HID_KEYBOARD_IDLE; hid_demo.state = HID_DEMO_KEYBOARD; //HID_KeyboardMenuProcess(); HID_KEYBD_Info_TypeDef *k_pinfo; char c; k_pinfo = USBH_HID_GetKeybdInfo(&hUSBHost); if(k_pinfo != NULL) { c = USBH_HID_GetASCIICode(k_pinfo); char str[5]; sprintf(str,'%c',c); HAL_UART_Transmit(&huart2,k_pinfo->keys,6,10000); } } }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Result (only
detected Not read data
)USB Device Attached PID: 1h VID: 258ah Address (#1) assigned. Manufacturer : SINO WEALTH Product : USB KEYBOARD Serial Number : N/A Enumeration done. This device has only 1 configuration. Default configuration set. Switching to Interface (#0) Class : 3h SubClass : 1h Protocol : 1h KeyBoard device found! HID class started.�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#usb-host #usb-hid #usb-stm32f205
Note: this post was migrated and contained many threaded conversations, some content may be missing.
Solved! Go to Solution.
2018-05-11 2:10 AM
Some time ago I applied the patch suggested by
pavel_a
and the stack worked fine but I had tried it with mice and keyboards. Now I need to send report to my custom device but I'm having some problems described in the following new forum question:https://community.st.com/0D50X00009XkX09SAF
Did you have similar issues?
2018-05-11 9:31 AM
Hi Luca,
I had to delay my project, sorry, have not tried yet. But in case I return to it, would like to know a solution.
Also would like to hear back from ST - any estimation when fixes to the USB library can be available, even as prevew?
-- pa
2018-05-14 7:15 AM
Yes, also USB library previews or patchs could be useful for me.
Thanks
2018-05-21 7:00 AM
Hello,
I would like to share with you a patch containing some improvements to deal with some buggy HID devices during enumeration phase. This patch will be deployed in a new version of the USB host library once validated.
If you can test it at your end using your failing devices, this will be helpful for us to validate the patch.
1-
STM32Cube_FW_F4_V1.0\Middlewares\ST\STM32_USB_Host_Library\Class\HID\Src\usbh_hid.c
: replace the implementation of USBH_HID_Process by the following:static USBH_StatusTypeDef USBH_HID_Process(USBH_HandleTypeDef *phost)
{
USBH_StatusTypeDef status = USBH_OK;
HID_HandleTypeDef *HID_Handle = (HID_HandleTypeDef *) phost->pActiveClass->pData;
switch (HID_Handle->state)
{
case HID_INIT:
HID_Handle->Init(phost);
case HID_IDLE:
status = USBH_HID_GetReport (phost, 0x01U, 0U, HID_Handle->pData, (uint8_t)HID_Handle->length);
if (status == USBH_OK)
{
fifo_write(&HID_Handle->fifo, HID_Handle->pData, HID_Handle->length);
HID_Handle->state = HID_SYNC;
}
else if (status == USBH_BUSY)
{
HID_Handle->state = HID_IDLE;
status = USBH_OK;
}
else if (status == USBH_NOT_SUPPORTED)
{
HID_Handle->state = HID_SYNC;
status = USBH_OK;
}
else
{
HID_Handle->state = HID_ERROR;
status = USBH_FAIL;
}
#if (USBH_USE_OS == 1U)
osMessagePut ( phost->os_event, USBH_URB_EVENT, 0U);
#endif
break;
case HID_SYNC:
...�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2-
STM32Cube_FW_F4_V1.0\Middlewares\ST\STM32_USB_Host_Library\Core\Src\usbh_ctlreq.c
: replace the implementation ofUSBH_CtlReq by the following:USBH_StatusTypeDef USBH_CtlReq (USBH_HandleTypeDef *phost,
uint8_t *buff,
uint16_t length)
{
USBH_StatusTypeDef status;
status = USBH_BUSY;
switch (phost->RequestState)
{
case CMD_SEND:
/* Start a SETUP transfer */
phost->Control.buff = buff;
phost->Control.length = length;
phost->Control.state = CTRL_SETUP;
phost->RequestState = CMD_WAIT;
status = USBH_BUSY;
#if (USBH_USE_OS == 1)
osMessagePut ( phost->os_event, USBH_CONTROL_EVENT, 0);
#endif
break;
case CMD_WAIT:
status = USBH_HandleControl(phost);
if (status == USBH_OK)
{
/* Commands successfully sent and Response Received */
phost->RequestState = CMD_SEND;
phost->Control.state =CTRL_IDLE;
status = USBH_OK;
}
else if (status == USBH_NOT_SUPPORTED)
{
/* Commands successfully sent and Response Received */
phost->RequestState = CMD_SEND;
phost->Control.state = CTRL_IDLE;
status = USBH_NOT_SUPPORTED;
}
else
{
if (status == USBH_FAIL)
{
/* Failure Mode */
phost->RequestState = CMD_SEND;
status = USBH_FAIL;
}
}
break;
default:
break;
}
return status;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Waiting for your feedback.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-05-21 11:23 AM
Amel,
With this patch both keyboard and mouse work, my hack no longer needed.
Thanks!
In USBH_HID_Process() line 9, I'd like to add possibility of error return from the class handler.Init (if the device does not have good report descriptors, or blacklisted, and so on):
case HID_INIT:
if (USBH_OK != HID_Handle->Init(phost)) { phost->gState = HOST_ABORT_STATE;break;
}(but still we have other unresolved problems with USB host. One is, immediately after unplugging keyboard or mouse, another (fake) attach event is received, and further real attachments are not detected).
- Pavel
2018-05-22 3:37 AM
Thanks
pavel_a
for your feedback.(but still we have other unresolved problems with USB host. One is, immediately after unplugging keyboard or mouse, another (fake) attach event is received, and further real attachments are not detected).
Are these problems described in separate discussion may be? If not, please do it in order to be able to follow the case efficiently?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-05-22 4:05 PM
Dear Amel,
These other issues are probably caused by our hardware (custom board). Sorry for the distraction.
No concrete facts yet.
Regards,
Pavel
2018-06-15 6:53 AM
Well I am trying to make this library work since march. The report function stop in the enumeration phase even with this last patch applied. Can someone help me?
Thanks
Kallil
2018-06-15 8:13 AM
Just to understand it better: have you the same problem in this my topic?
2018-06-15 8:57 AM
It's the same problem as your Typhoon mouse