2024-05-12 2:08 AM
Hello everyone.
I am working on a project which needs low level access to USB mass storage class such as reading sector size/count of an attached storage device but thus far I could not get anything out of my board which is nucleo-f446re.
I have initialized my board as a USB host mass storage class and I am abled to write on specific sectors such as sector number 10 and it DOES write it down using msc_scsi.c functions but I can't find any solution to determine sector count of attached device. I just can't find the appropriate function/data structure for it,
Can anyone please help me with it?
2024-05-12 8:54 AM
SCSI command READ CAPACITY doesn't work as it always returns 0.
Should I initialize something first? And if yes, how to do so?
I'm not using fatfs middleware so I guess lots of data structures are not initialized automatically.
2024-05-12 9:14 AM
Also it might be worth noting that phost->pActiveClass->pData is equal to 0 which means null pointer and when I make a call to any function that uses this particular data, the micro hangs completely. That's why I think I'm missing some initialization steps.
However phost->pData is set and can be referenced, but it doesn't contain the valid data I'm looking for.