USB Host Bulk Input NAK || STM32U575
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-07 10:43 AM
Hi All,
I am working on the STM32U575 for host mass storage class.
I am not using stm32 middle ware for this due to some reasons.
I am using TinyUSB open-source stack to implement the Host mass storage class.
with my current implementation I am able to use HID device, but I got stuck at MSC enumeration.
Currently facing below issue.
1. During enumeration process After sending the Unit Test Ready Command I am getting correct CSW
response from device but soon after that Getting NAK from USB device.
-- What could be the reasons for getting the NAK - Also I after getting NAK I am continuously getting Channel halted interrupt.
I have attached the logic analyzer file for batter understanding.
Any Help will be highly appreciated!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-13 3:12 AM
Hi, any one from ST can please respond to above query? It will be great help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-08-13 4:58 AM
Dear @RRajb.2 ,
a NAK means the Firmware stack not able to respond in required timing to an IN packet, so most probably the state machine of the stack seems in a wrong state before or when responding to the Unit Test ready command , therefore all next transactions are halted . I would suggest to try to comment that command in the stack for debugging purposes and see if the issue is happening in the command just before ? Another check to use another USB key or any other mass storage device to check if such commands are supported. I’m not expert of USB just to give some pointers. Hope it helps you.
Ciao
STOne-32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-12 10:50 PM
Did you find a reason for this?
I am seeing exactly the same thing, basically the second command always fails.
I can Send "Unit test ready", works fine. Then send it again and just NAKs.
Cheers
Andy
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-12 11:01 PM
ACapo.1 not sure if the root cause will be same for you or not? as in my case I was using our own implementation for developing low level USB drivers, we were not using cube MX.
but any how, the root cause was related to the size of data bytes. as after unit test ready command, when we were trying to send next command which was having data bytes more then 256 bytes, USB device was giving NAK.
to overcome this issue, we were sending the data in chunk of 256 bytes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-12 11:09 PM
Hi @RRajb.2
Thanks for the super fast response.
Looks like it is possibly a different issue then as I have a test setup here just sending the same command twice.
Driving me mad!
Thanks
Andy
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-13 1:26 AM
which code are you using??? CubeMX generated code?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-13 1:34 AM - edited ‎2023-12-13 1:35 AM
The HAL_HCD_HC_ stuff.
So the TinyUSB hcd code is using:
HAL_HCD_Init
HAL_HCD_Start
HAL_HCD_HC_Init
HAL_HCD_HC_SubmitRequest
And the following callbacks:
HAL_HCD_Connect_Callback
HAL_HCD_Disconnect_Callback
HAL_HCD_SOF_Callback
HAL_HCD_HC_NotifyURBChange_Callback
Interestingly I have just tested a midi controller using BULK EPs and that is working fine.
The example TinyUSB MSC example though is not working.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-13 1:47 AM
Okay so you are also using the same tinyUSB stack, so Mostly you might have used the same driver file which I used.
STM32F7xx Host driver (github.com)
I was also able to use the MIDI initially and then facing the issue with bulk driver only.
for tinyUSB driver file you should handle data in chunk for length more then 256 byte.
Also
under HAL_HCD_HC_NotifyURBChange_Callback function()
currently endpoint toggle is unconditional,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-13 2:50 AM
Thanks very much for the help on this.
Yes I based it on that code, changed slightly for the H7
The ep->toggle is currently conditional in HAL_HCD_HC_NotifyURBChange_Callback(), or are you saying it should be in _endpoint_xfer() as well?
Not transferring > 256 either, currently I have it forced to FS so it is dealing with 64 byte packets. Unless I am misunderstanding?
SCSI Test Unit Ready
[1] Claimed EP 0x02
Queue EP 02 with 31 bytes ...
hcd_edpt_xfer on pipe for devaddr:1 epaddr:02 in slot 8, ep_type 2, ep_dir 0, len 31
***** HAL_HCD_HC_Init ch_num = 8, epnum = 2, dev_address = 1, speed = 1, ep_type = 2, mps = 64
***** HAL_HCD_HC_SubmitRequest ch_num = 8, direction = 0, type = 2, token = 1, length = 31, do_ping = 1
BULK OUT
55 53 42 43 42 53 55 54 00 00 00 00 00 00 06 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
OK
Transfer SUCCESS devaddr 01 ep:02 31 bytes, channel 8
on EP 02 with 31 bytes: OK
MSC xfer callback
Queue EP 81 with 13 bytes ...
hcd_edpt_xfer on pipe for devaddr:1 epaddr:81 in slot 7, ep_type 2, ep_dir 1, len 13
***** HAL_HCD_HC_Init ch_num = 7, epnum = 129, dev_address = 1, speed = 1, ep_type = 2, mps = 64
***** HAL_HCD_HC_SubmitRequest ch_num = 7, direction = 1, type = 2, token = 1, length = 13, do_ping = 1
BULK IN
OK
Transfer SUCCESS devaddr 01 ep:81 13 bytes, channel 7
on EP 81 with 13 bytes: OK
MSC xfer callback
SCSI Read Capacity
[1] Claimed EP 0x02
Queue EP 02 with 31 bytes ...
hcd_edpt_xfer on pipe for devaddr:1 epaddr:02 in slot 8, ep_type 2, ep_dir 0, len 31
***** HAL_HCD_HC_Init ch_num = 8, epnum = 2, dev_address = 1, speed = 1, ep_type = 2, mps = 64
***** HAL_HCD_HC_SubmitRequest ch_num = 8, direction = 0, type = 2, token = 1, length = 31, do_ping = 1
BULK OUT
55 53 42 43 42 53 55 54 08 00 00 00 80 00 0a 25
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
OK
Transfer SUCCESS devaddr 01 ep:02 31 bytes, channel 8
on EP 02 with 31 bytes: OK
MSC xfer callback
Queue EP 81 with 8 bytes ...
hcd_edpt_xfer on pipe for devaddr:1 epaddr:81 in slot 7, ep_type 2, ep_dir 1, len 8
***** HAL_HCD_HC_Init ch_num = 7, epnum = 129, dev_address = 1, speed = 1, ep_type = 2, mps = 64
***** HAL_HCD_HC_SubmitRequest ch_num = 7, direction = 1, type = 2, token = 1, length = 8, do_ping = 1
BULK IN
OK
So that is what I see with the MSC example