2024-01-23 02:27 AM
I bought an STM32F072 disco board specifically to develop a USB CDC application, but I can't now find an example or demo in STM32CubeMX V6.10. I found this thread https://community.st.com/t5/stm32-mcus-products/stm32f070-usb-cdc-example/m-p/457994#M150836 but has this dropped out of Cube 6.10?
Solved! Go to Solution.
2024-01-23 02:31 AM
2024-01-23 02:31 AM
2024-01-23 03:01 AM - edited 2024-01-23 04:06 AM
Thanks, just what I was looking for. Sadly it doesn't compile.....
The IAR IDE wont even open some of the files, says it includes an invalid path. Maybe I can fix that.
Update, the folders for the Cube drivers I downloaded from github were all empty, no idea why. I had to download them more or less separately and then patch the include paths to point to where I'd put them. It now compiles!
2024-01-23 07:01 AM
God these examples are so frustrating! They look CubeMX generated but don't include the CubeMX file so they are almost impossible to modify. I can't even determine the pins used without reverse engineering the C source.
2024-01-23 07:45 AM
Jan, as ever, you're a star. I'm going to start a new thread to get help with this example.