cancel
Showing results for 
Search instead for 
Did you mean: 

USB CDC and MSC Middlewares integration

Ghada Dhibi
Associate II
Posted on July 27, 2017 at 13:13

Hi all, 

I'm using STM32L486 microcontoler and USB device. 

Using MSC_Standalone and CDC_Standalone project example from the STM32Cube I was able to configure the USB device on CDC and MSC. 

Now, I want to integrate both of example on the same project, and depending on the main application, I have to choose the usb configuration to work with. 

Is there any USB device example working on both of configurations ? 

Warnings and errors occurs when I Intergate both of them. 

Thanks. 

#stm32l4 #usb #usb-cdc #usb-msc-fat #stm32l4-usb
1 REPLY 1
Imen.D
ST Employee
Posted on July 27, 2017 at 22:37

Hi Ghada,

Refer to this discussion, it may help you

https://community.st.com/0D50X00009Xkh8FSAR

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen