2024-12-30 01:26 PM
Dear Community,
I have an reocurring issue with STM32G4 series processors:
I am programming via UART from another embedded system. Via this system, I can set Boot0 pin and NRST as well as communicate via UART.
When the STM is flashed via CubeProg on another port, I can enter the bootloader mode, send magic byte and receive ACK.
Then I can proceed to do a mass erase. I can see via CubeProg, that the mass erase is successful.
However, I can neither continue to write nor get back into the bootloader mode via the same pin toggeling succesfully. While I can see from the external pin states, that bootloader mode is loaded, I do not get any ACK on the magic byte anymore.
Even a power cycle does not change the outcome.
As soon as I flash again via CubeProg, I can enter and leave the bootloader mode sucessfully again using BOOT0 and NRST.
All Option Bytes are default, and also no read or write protection set up.
I am at a loss here, any suggestions on how this behaviour could be debugged?
2025-01-22 06:10 AM
Dear @mniethammer ,
Can you please provide more details on this :
When the STM is flashed via CubeProg on another port, I can enter the bootloader mode, send magic byte and receive ACK. Then I can proceed to do a mass erase. I can see via CubeProg, that the mass erase is successful."
You are using SWD and Programming the MCU or using Bootloader with ST-Link , if possible to provide the Serial/RS232 trace of the failure to see if a NACK or a timeout ?
Thank you
STOne-32.