2019-05-19 9:28 AM
The DFSDM section 29.7 channel configuration register has an offset for each channel of 0x20*y while the SVD file has a 0x4 offset between the channels. Can somebody state the correct offset?
SVD:
...
<name>DFSDM_CHCFG0R1</name>
<displayName>DFSDM_CHCFG0R1</displayName>
<description>DFSDM channel configuration 0 register
1</description>
<addressOffset>0x0</addressOffset>
.....
<name>DFSDM_CHCFG1R1</name>
<displayName>DFSDM_CHCFG1R1</displayName>
<description>DFSDM channel configuration 1 register
1</description>
<addressOffset>0x4</addressOffset>
.h
...
#define DFSDM1_Channel0_BASE (DFSDM1_BASE + 0x00)
#define DFSDM1_Channel1_BASE (DFSDM1_BASE + 0x20)
#define DFSDM1_Channel2_BASE (DFSDM1_BASE + 0x40)
#define DFSDM1_Channel3_BASE (DFSDM1_BASE + 0x60)
#define DFSDM1_Channel4_BASE (DFSDM1_BASE + 0x80)
#define DFSDM1_Channel5_BASE (DFSDM1_BASE + 0xA0)
#define DFSDM1_Channel6_BASE (DFSDM1_BASE + 0xC0)
#define DFSDM1_Channel7_BASE (DFSDM1_BASE + 0xE0)
-Z
2019-05-31 5:40 AM
Hello @Sigbjørn Kolberg ,
You are right, the svd file is wrong.
We raised this issue internally for fix in the coming release.
Thanks for highlighting this issue.
Best Regards,
Imen
2019-09-06 6:26 AM
Any signs of this fix coming soon? I'm porting code from an F4 to an H7 and really need to see what's happening in the DFSDM system.
Regards,
Jason
2019-12-11 7:14 AM