cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 SystemIsolation_Config

jrocher-althea
Associate

 

Hello all,

I'm working with the STM32N6 series and I'm trying to correctly configure the isolation between the secure and non-secure domains using the RIF (Runtime Isolation Framework).

I found example code like this in a template (STM32CubeN6)

 
static void SystemIsolation_Config(void) { /* USER CODE BEGIN RIF_Init 0 */ /* USER CODE END RIF_Init 0 */ /* set all required IPs as secure privileged */ __HAL_RCC_RIFSC_CLK_ENABLE(); RIMC_MasterConfig_t RIMC_master = {0}; RIMC_master.MasterCID = RIF_CID_1; RIMC_master.SecPriv = RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_PRIV; /*RIMC configuration*/ HAL_RIF_RIMC_ConfigMasterAttributes(RIF_MASTER_INDEX_ETH1, &RIMC_master); /*RISUP configuration*/ HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_ADC12 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_CSI , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_ETH1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_I2C1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_I2C2 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_ICACHE , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_LPUART1 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_XSPI2 , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); HAL_RIF_RISC_SetSlaveSecureAttributes(RIF_RISC_PERIPH_INDEX_XSPIM , RIF_ATTRIBUTE_SEC | RIF_ATTRIBUTE_NPRIV); /* RIF-Aware IPs Config */ /* set up GPIO configuration */ HAL_GPIO_ConfigPinAttributes(GPIOA,GPIO_PIN_10,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOA,GPIO_PIN_11,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_0,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_3,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_6,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_7,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_10,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOB,GPIO_PIN_11,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOC,GPIO_PIN_1,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOE,GPIO_PIN_3,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOE,GPIO_PIN_6,GPIO_PIN_SEC|GPIO_PIN_NPRIV); HAL_GPIO_ConfigPinAttributes(GPIOH,GPIO_PIN_9,GPIO_PIN_SEC|GPIO_PIN_NPRIV); /* USER CODE BEGIN RIF_Init 1 */ /* USER CODE END RIF_Init 1 */ /* USER CODE BEGIN RIF_Init 2 */ /* USER CODE END RIF_Init 2 */ }
View more

However, I’m unclear on:

  1. How to correctly configure GPIOs/Periphals used by non-secure applications.

  2. Whether there’s an official list or documentation for the STM32N6 that shows all RIF-aware peripherals and their indices (like RIF_RISC_PERIPH_INDEX_*).

  3. Any guidance or reference templates for properly setting up the isolation for a basic non-secure application (e.g., accessing UART and I2C from non-secure code).

Any help or pointers to documentation specific to STM32N6 and TrustZone+RIF configuration would be greatly appreciated!

Thanks in advance.

1 REPLY 1
Saket_Om
ST Employee

Hello @jrocher-althea 

Could you check the example below please:

Projects/NUCLEO-N657X0-Q/Examples/RIF/RIF_Peripheral

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om