cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 FreeRTOS: undefined reference to `MPU_xTaskCreate'` error

milanvdm
Associate II

@Saket_Om This solved the privileged calls but Im hitting the next obstacle with `undefined reference to `MPU_xTaskCreate'`.

Im creating a task using `xTaskCreate` which gets redefined at https://github.com/STMicroelectronics/x-cube-freertos/blob/b0f4a6681bd37b483076db2e8171239db9dacbb1/Middlewares/Third_Party/FreeRTOS/Source/include/mpu_wrappers.h#L100.

From what I gather, this `MPU_xTaskCreate` is defined at https://github.com/STMicroelectronics/x-cube-freertos/blob/b0f4a6681bd37b483076db2e8171239db9dacbb1/Middlewares/Third_Party/FreeRTOS/Source/include/mpu_prototypes.h

I have added the `include` folder into my GCC compiler path so not sure why it would not be able to find the `MPU_xTaskCreate`?

 

milanvdm_0-1735483477673.png

 

5 REPLIES 5
Saket_Om
ST Employee

Hello @milanvdm 

Is this flag "configUSE_MPU_WRAPPERS_V1" is set to 1 on your project?

Compiler cannot find "MPU_xTaskCreate" if this flag is not set to 1.

#if ( configUSE_MPU_WRAPPERS_V1 == 1 )

    BaseType_t MPU_xTaskCreate( TaskFunction_t pxTaskCode,
                                const char * const pcName,
                                const uint16_t usStackDepth,
                                void * const pvParameters,
                                UBaseType_t uxPriority,
                                TaskHandle_t * const pxCreatedTask ) FREERTOS_SYSTEM_CALL;
 

 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar
milanvdm
Associate II

This is the follow-up of the issue in the link below:

Solved: Re: STM32N6 FreeRTOS linker issue for MPU - STMicroelectronics Community

 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar
milanvdm
Associate II

@Saket_Om Were you able to reproduce this issue or do you need more information?

Hello @milanvdm 

The issue is under investigation. We will get back to you as soon as possible.

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar