2017-06-28 2:51 AM
I am experiencing some troubles with STM32L432KC USB Bootloader. I am using DfuSe Demo v3.0.5 to upgrade firmware.
DFuSe firmware upgrade fails in 95% of situations. Both on our STM32L432KC project and on Nucleo-32 STM32L432 evaluation board. Also tried to upgrade with sample project hex files provided by ST. Same result.
Error Code: Bad state machine in firmware
TransferSize: 2048
DFU State: STATE_IDLE
DFU Status: STATUS_OK
Request: Get Status Request.
CurrentNBlock: 0x0000
CurrentLengths: 0x0005
Percent: 24% (may differ)
Thank you in advance.
#firmware-upgrade #usb-bootloader #nucleo-32-stm32l432 #stm32l432kc #dfuse #bootloader-firmware-upgrade2017-11-10 4:42 AM
I have the same problem. Any update on that?
2018-04-22 5:11 AM
I have had the same issue on Windows 8 (x64).
I've tried it just now on my home computer (Windows 7 x64) and it seems to work there. Might be the OS then?
2018-05-18 5:02 AM
I have the same problem. any update?
I cant find a solution...
synchronization problem?
(I have Win7 x64 and the problem occurs)
2018-05-18 10:09 AM
Unfortunately no, but the problem must have something to do with the computer (at least in my case).
2018-06-21 6:36 AM
I compiled the source code for the DFUSe (downloadable from ST) using visual studio 2013.
I added a Sleep(20) to sleep for 20 ms inside the loop in function
CSTThread
::BodyThread().Now the function no longer seems to have that error (suggesting that it's a race hazard between threads).
I have a ticket open with ST on the issue but i hope this helps until they solve the issue.
Regards
PS: 20 is a random number that works. i tried 1, 5 and 10 without much luck. Feel free to optimize away, or to select a larger number in case you don't mind waiting (the sleep is called at every sub-step of the erase/flash process)