2021-04-22 1:57 AM
I am Using STM32L412CBT6 controller in that the application working with a regular power supply 2.8 volts but with a battery the remianing modules(i2c/RTC) but in SPI F-open is not working
2021-04-22 5:45 PM
Hello
Used LDO is for 200mA . Is the current in mA consumed by the SD card (as per user manualn) less than (200- Imcu)? Imcu is the MCU operation current
Check the 2.8V rail for voltage drop during SD transactions.