2015-04-18 2:00 PM
Hi,
I am not able to program the flash of a STM32L151RC using ''half page'' programming.Normal programming (word by word) works fine.I have tried it using the 2 latest GCC compilers (4.8.4), and I have tried with the 2 latest HAL drivers (1.1.0 and 1.1.1).The code below stops working when the 32 words are being written to flash. The debugger stops working. When running the code without a debugges, it also doesn't work.Am I the only one with this observation?Best regardsMartinHAL_FLASH_Unlock();__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_WRPERR);__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_PGAERR);__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_SIZERR);__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERRUSR);__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_RDERR);uint32 data[32] = { 0 };if (HAL_FLASHEx_HalfPageProgram(0x08004000, data) == HAL_OK){// Success}else{// Error} #stm32l-hal-driver-flash-write #iap-flash-half-page-program2016-01-12 2:22 PM
I ran into a similar issue while developing a IAP bootloader for a stm32L1 device. I was modifying an existing bootloader for an F1 device, and found that on the L1 device the flash writes took far too long in word program mode. I tried the HAL_FLASHEx_HalfPageProgram function, but it only seemed to crash.
As I found, this is because the hal library __ramfunc macro (for gcc) tries to place the function in a memory section called '.RamFunc' which does not exist in the standard linker script for the stm32. I modified my linker script to include a .Ramfunc section in the .data block, and it now works fine. Hope this helps someone2016-06-27 12:12 AM
Hi,
I am also having some issues with using HAL_FLASHEx_HalfPageProgram()I have my bootloader and my application in Memory bank1, and my downloaded image in memory bank 2. In bootloader I am trying to write in memory bank 1 (application) , the data located in memory bank 2 (downloader image).but this process is not working. I am constantly having a PGAERR error. This is the code: numBytes = 237568, address=0x08006000if (((numBytes % 128) == 0) && ((address % 0x80) == 0)){ uint32_t* pDataByte = (uint32_t*)pDataToWrite; TerminalSend_Str_NL(''Writing half page''); // Half Page flash write is 128 bytes (and in multiple of 128-bytes) if (HAL_FLASHEx_HalfPageProgram(address, (uint32_t*) pDataByte) != HAL_OK) { TerminalSend_Str_Hexu32_NL(''HAL Flash Half Page Write Error: '', HAL_FLASH_GetError()); }}And my linker file: /* Initialized data sections goes into RAM, load LMA copy after code */ .data : { . = ALIGN(4); _sdata = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ *(.RamFunc) /* .RamFunc sections */ . = ALIGN(4); _edata = .; /* define a global symbol at data end */ } >RAM AT> FLASHDo you have any idea what could be wrong?Regards,B.2016-12-09 9:32 PM
I have the exact same problem. I'm using Ramfunc properly. I can avoid the PGAERR if I only write 8 bytes, e.g.
/* Write one half page directly with 32 different words */
while(count < 2) // was 32But not very satisfactory. :)
Did you solve this problem? I'm on an STM32L151xE.
Thanks,
G.
2017-01-06 12:50 AM
Hi,
Could you please try to update the HAL_FLASHEx_HalfPageProgram() function as below:
/* Disable all IRQs */
__disable_irq();
/* Write one half page directly with 32 different words */
while(count < 32)
{
*(__IO uint32_t*) ((uint32_t)(Address + (4 * count))) = *pBuffer;
pBuffer++;
count ++;
}
/* Wait for last operation to be completed */
status = FLASHRAM_WaitForLastOperation(FLASH_TIMEOUT_VALUE);
/* Enable IRQs */
__enable_irq();�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Please try with this update, and tell us about the result.
-Nesrine-
Ifmy suggestanswers your question, please mark it as correct.
2017-01-06 11:51 AM
You've added disable/enable_irq()... yes, I think that was one of my problems. Surprisingly in the voluminous but mostly useless boilerplate documentation, no mention or reminder about IRQs in any of the 3 stm32l1xx_hal_flash_*.c files.
I see you've maintained ridiculous coding convention of commenting on a properly named function. The useless verbosity is a hindrance to readability. A comment that says 'disallow interrupts so we don't cause a flash wait-state resulting in a PGAERR' would be ideal. And this original comment:
/* Write one half page directly with 32 different words */
So one is not allowed to write 32 identical words? Where's the check for that? :)
2017-01-27 3:29 AM
The STM32L0 library does include interrupt handling:
__RAM_FUNC HAL_FLASHEx_HalfPageProgram(uint32_t Address, uint32_t *pBuffer)
{ uint32_t count; HAL_StatusTypeDef status;/* Wait for last operation to be completed */
status = FLASHRAM_WaitForLastOperation(FLASH_TIMEOUT_VALUE);if(status == HAL_OK)
{ /* Proceed to program the new half page */ SET_BIT(FLASH->PECR, FLASH_PECR_FPRG); SET_BIT(FLASH->PECR, FLASH_PECR_PROG); count = 0U; /* Write one half page, Address doesn't need to be increased *//* Disable all IRQs */
__disable_irq();while(count < 16U)
{ *(__IO uint32_t*) Address = *pBuffer; pBuffer++; count++; }/* Enable IRQs */
__enable_irq(); /* Wait for last operation to be completed */ status = FLASHRAM_WaitForLastOperation(FLASH_TIMEOUT_VALUE);/* If the write operation is completed, disable the PROG and FPRG bits */
CLEAR_BIT(FLASH->PECR, FLASH_PECR_PROG); CLEAR_BIT(FLASH->PECR, FLASH_PECR_FPRG); } /* Return the write status */ return status;}2017-01-27 8:45 AM
Lucky you... the code I inherited does not have this.
* @file stm32l1xx_hal_flash_ramfunc.c
* @author MCD Application Team * @version V1.1.3 * @date 04-March-2016 * @brief FLASH RAMFUNC driver.