cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7S78-DK pll3 periph error for lcd

hamzatamer
Associate II

I tried the bsp example among the examples of the stm32 h7s78-dk board. I integrated it into my own code. My aim is to use the LCD screen and broadcast the camera output on it. In the first stage, I try to print any text on the screen. The BSP example code works but cannot be debugged. I also get an error about pll3 when trying to initialize lc in my own code. I have shared the reasons for the error step by step in the pictures while debugging.

hamzatamer_0-1733824321085.pnghamzatamer_1-1733824397807.png

 

hamzatamer_4-1733824441527.png

hamzatamer_5-1733824451590.png

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

here is to solution, if you want to run examples first you have to configure debug and startup settings. if you use stm32h7s78-dk or similar card you should keep in mind that it is a card with an external loader. First, add external loader in debug settings, after that, If you do not have a boot project, add the BOOT_XIP.hex file to the startup under the binary folder in the Templates folder and move the following line, i.e. move down also uncheck load symbols

View solution in original post

3 REPLIES 3

Please see the Posting Tips for how to properly post source code - not as images:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228 

 


@hamzatamer wrote:

The BSP example code works but cannot be debugged.


What do you mean by that?

 

some stm32h7s78-dk's examples are not working, for example BSP,LTDC_Display_2Layers,LTDC_ColorKeying. Error is in common.

if ((RCC->PLLCKSELR & RCC_PLLCKSELR_PLLSRC) != pllsrc) { /* There is another PLL activated with another source */ return HAL_ERROR; }


this area returns HAL_ERROR i dont know why it is example code. I don't change anything. I open the code from the examples section and debug it. and it gets stuck at the HSI section. I get this error on samples that include LCD screens

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_NONE; RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE; RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL3.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL3.PLLM = 4; RCC_OscInitStruct.PLL3.PLLN = 25; RCC_OscInitStruct.PLL3.PLLP = 2; RCC_OscInitStruct.PLL3.PLLQ = 20; RCC_OscInitStruct.PLL3.PLLR = 16; RCC_OscInitStruct.PLL3.PLLS = 2; RCC_OscInitStruct.PLL3.PLLT = 2; RCC_OscInitStruct.PLL3.PLLFractional = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { /* Initialization error */ while(1); } PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LTDC; PeriphClkInit.LtdcClockSelection = RCC_LTDCCLKSOURCE_PLL3R;

 

here is to solution, if you want to run examples first you have to configure debug and startup settings. if you use stm32h7s78-dk or similar card you should keep in mind that it is a card with an external loader. First, add external loader in debug settings, after that, If you do not have a boot project, add the BOOT_XIP.hex file to the startup under the binary folder in the Templates folder and move the following line, i.e. move down also uncheck load symbols