cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7S3L8 - is there any example to flash firmware to external memory using spi and execute in place

AnoopYadav
Associate

Is there any example to flash firmware image to external flash memory over SPI and execute in place.

Device - STM32H7S3L8

1 REPLY 1
Saket_Om
ST Employee

Hello @AnoopYadav 

 

Please refer to the QSPI example provided in STM32CubeH7. 

This Application Note AN4760 provides detailed information on the Quad-SPI interface on STM32 microcontrollers and microprocessors. It includes examples and guidelines for configuring and using the QSPI interface for executing code from external flash memory.

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar