cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747 - I2S Fullduplex with DMA is not working

MichaelZemah
Associate II

I'm trying to build an audio project using STM32H747 MCU.

I wish to configure the cortex M7 to process the audio in and out buffers.

I'm trying to work with double buffers of input and output. the DMA should handle the transactions to and from the i2s peripheral.

 

HAL_I2SEx_TransmitReceive_DMA(&hi2s2, (uint16_t*)&outBuffer[0][0], (uint16_t*)&inBuffer[0][0], AUDIO_BUFFER_U16_STREAMS/4);

 

and the half & full complete callbacks are:

void HAL_I2SEx_TxRxHalfCpltCallback (I2S_HandleTypeDef *hi2s) {

pInBuffer = &inBuffer[0][0];

pOutBuffer = &outBuffer[0][0];

// SCB_CleanDCache();

// SCB_InvalidateDCache();

dataReadyFlag = true;

}

 

void HAL_I2SEx_TxRxCpltCallback (I2S_HandleTypeDef *hi2s) {

pInBuffer = &inBuffer[1][0];

pOutBuffer = &outBuffer[1][0];

// SCB_CleanDCache();

// SCB_InvalidateDCache();

dataReadyFlag = true;

}

 

and all I'm doing in the super loop is to copy the input to the output when I have dataReadyFlag == true.

 

I hooked all the I2S lines to a data logger and the peripheral seems to work.

but whenever I get a new buffer from DMA it is Empty and all set to '0'.

 

Why this is happening ?

please help me with e full explanation on how to fix this.

as you can see I already tried setting the buffer to a specific RAM location to prevent DMA and Catch issues but it didn't help. maybe I did it wrong.

 

8 REPLIES 8
TDK
Guru

A few things to consider:

If you feel a post has answered your question, please click "Accept as Solution".

OK so just to be clear,

the catch is disabled
my code is attached
here is what I've added to the Flash.ld file:

 

.ram2Block (NOLOAD) :

{

KEEP (*(.MY_RAM_D2))

} > RAM_D2

then I defined the buffers:

__attribute__ (( section(".MY_RAM_D2") )) uint16_t inBuffer[2][AUDIO_BUFFER_SIZE_U16_ARRAY] = {0};

__attribute__ (( section(".MY_RAM_D2") )) uint16_t outBuffer[2][AUDIO_BUFFER_SIZE_U16_ARRAY] = {0};

__attribute__ (( section(".MY_RAM_D2") )) volatile uint16_t* pInBuffer = &inBuffer[1][0];

__attribute__ (( section(".MY_RAM_D2") )) volatile uint16_t* pOutBuffer = &outBuffer[1][0];

 

still not working

MichaelZemah
Associate II

I request ST's employe's help, and exact explenation and instructions on what to do to make the STM32H747 work with fullduplex I2S and DMA stream, i.e: HAL_I2Sex_TransmitRecieveDMA.

 

It's ST's FLAGSHIP MCU and it's simpely not working out of the box.

TDK
Guru

Note that this is primarily a user run forum, not a direct link to ST support.

You can initiate an online support request here:

https://www.st.com/content/st_com/en/support/support-home.html

If you feel a post has answered your question, please click "Accept as Solution".

i have it working, on H743 (almost same cpu, but only H7 core) . and it was working "out of the box". in 16bit data mode.

just in 32bit mode it didnt work with my dac, so i use SAI , the "better" I2S connection.

 

btw i use circular buffers, 4096 x int16  size .

If you feel a post has answered your question, please click "Accept as Solution".
LCE
Principal II

I'm using I2S / SAI DMA on H723 and H735 in DBM mode, running smoothly for hours.

Show your DMA setup.

Often, it is the DMA's width setting. For a start, use half-word (16bit) or word (32bit) in both directions.

And I think I had to modify the HAL DMA start function in DBM mode.

LCE
Principal II

Better reply than edit your first post.

Anyway... so you are not using DBM mode, with double buffer you mean you are using 2 buffers?

Here:

HAL_I2SEx_TransmitReceive_DMA(&hi2s2, (uint16_t*)&outBuffer[0][0], (uint16_t*)&inBuffer[0][0], AUDIO_BUFFER_U16_STREAMS/4);

DMA always reads & writes to xBuffer[0], it will never ever use xBuffer[1], but in the complete callback pointers are set to xBuffer[1].

You should start with RX buffer all the same values (something recognisable like 0xA5A5, but neither 0 nor 0xFFFF),
then fill your TX buffer with e.g. "i++".
Then, as a start, leave out any other hardware and directly connect I2S data in and out.

For debugging, don't copy anything, just check your RX buffer, which should be equal to TX buffer.

I believe it was moved by Amel, which triggers the notification. Don't think the OP has been back since the original couple replies.

If you feel a post has answered your question, please click "Accept as Solution".