cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h743zit6 internal temperature sensor

ram_1
Associate

I am using stm32h743zitx nucleo board and thermal camera ,but in nucleo board stm32h743zitx internal temperature came 32 to 35 degree but same code i am using thermal camera than stm32h743zitx internal temperature came 123 and going above degree why i upload my code below please give me sollution where is my problem .i am using both 400 Mhz clock ....

float temperature;
uint32_t temperature_1 = 0;
uint32_t adcValue = 0;
uint32_t vrefint = 0;
uint32_t temp_sensor = 0;
 
float vrefint_volts;
float temperature_celsius;
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */
  

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  MX_ADC3_Init();

  while (1)
    {
        temperature = Get_Temperature(&vrefint_volts, &temperature_celsius);
        // Use the temperature value as needed
        HAL_Delay(1000);
    }

}
uint32_t Get_Temperature(float *vrefint_volts, float *temperature_celsius)
{
    
     HAL_ADCEx_Calibration_Start(&hadc3, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
	  HAL_Delay(100);
    // Start ADC conversion for temperature sensor
    HAL_ADC_Start(&hadc3);
    if (HAL_ADC_PollForConversion(&hadc3, 100) == HAL_OK)
    {
        temp_sensor = HAL_ADC_GetValue(&hadc3);
    }
    HAL_ADC_Stop(&hadc3);

    // Read the calibration values
    uint16_t cal1 = *TEMPSENSOR_CAL1_ADDR;
    uint16_t cal2 = *TEMPSENSOR_CAL2_ADDR;
    uint16_t vrefint_cal = *VREFINT_CAL_ADDR;

    // Calculate the analog reference voltage (Vref+) in millivolts
    vrefint = __HAL_ADC_CALC_VREFANALOG_VOLTAGE(vrefint_cal, ADC_RESOLUTION_16B);
    *vrefint_volts = vrefint / 1000.0f;  // Convert millivolts to volts

//    // Calculate temperature in degrees Celsius
   *temperature_celsius = (float)__HAL_ADC_CALC_TEMPERATURE(vrefint, temp_sensor, ADC_RESOLUTION_16B);
    return (uint32_t)*temperature_celsius;
}

ADC_HandleTypeDef hadc3;

/* ADC3 init function */
void MX_ADC3_Init(void)
{
    ADC_ChannelConfTypeDef sConfig = {0};

    /* Configure ADC3 peripheral */
    hadc3.Instance = ADC3;
    hadc3.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV6;
    hadc3.Init.Resolution = ADC_RESOLUTION_16B; // ADC resolution for internal temperature sensor
    hadc3.Init.ScanConvMode = ADC_SCAN_DISABLE;
    hadc3.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
    hadc3.Init.LowPowerAutoWait = DISABLE;
    hadc3.Init.ContinuousConvMode = DISABLE;
    hadc3.Init.NbrOfConversion = 1;
    hadc3.Init.DiscontinuousConvMode = DISABLE;
    hadc3.Init.ExternalTrigConv = ADC_SOFTWARE_START;
    hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
    hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
    hadc3.Init.Overrun = ADC_OVR_DATA_PRESERVED;
    hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
    hadc3.Init.OversamplingMode = DISABLE;
    if (HAL_ADC_Init(&hadc3) != HAL_OK)
    {
        Error_Handler();
    }

    /* Configure the ADC channel for temperature sensor */
    __HAL_RCC_VREF_CLK_ENABLE(); // Enable VREFINT clock
    sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
    sConfig.Rank = ADC_REGULAR_RANK_1;
    sConfig.SamplingTime = ADC_SAMPLETIME_810CYCLES_5;
    sConfig.SingleDiff = ADC_SINGLE_ENDED;
    sConfig.OffsetNumber = ADC_OFFSET_NONE;
    sConfig.Offset = 0;
    if (HAL_ADC_ConfigChannel(&hadc3, &sConfig) != HAL_OK)
    {
        Error_Handler();
    }
}

#define VREFINT_CAL_ADDR                   ((uint16_t*) (0x1FF1E860UL)) /* Internal voltage reference, address of parameter VREFINT_CAL: VrefInt ADC raw data acquired at temperature 30 DegC (tolerance: +-5 DegC), Vref+ = 3.3 V (tolerance: +-10 mV). */
#define VREFINT_CAL_VREF                   (3300UL)                     /* Analog voltage reference (Vref+) value with which temperature sensor has been calibrated in production (tolerance: +-10 mV) (unit: mV). */
/* Temperature sensor */
#define TEMPSENSOR_CAL1_ADDR               ((uint16_t*) (0x1FF1E820UL)) /* Internal temperature sensor, address of parameter TS_CAL1: On STM32H7, temperature sensor ADC raw data acquired at temperature  30 DegC (tolerance: +-5 DegC), Vref+ = 3.3 V (tolerance: +-10 mV). */
#define TEMPSENSOR_CAL2_ADDR               ((uint16_t*) (0x1FF1E840UL)) /* Internal temperature sensor, address of parameter TS_CAL2: On STM32H7, temperature sensor ADC raw data acquired at temperature 110 DegC (tolerance: +-5 DegC), Vref+ = 3.3 V (tolerance: +-10 mV). */
#define TEMPSENSOR_CAL1_TEMP               (30L)                        /* Internal temperature sensor, temperature at which temperature sensor has been calibrated in production for data into TEMPSENSOR_CAL1_ADDR (tolerance: +-5 DegC) (unit: DegC). */
#define TEMPSENSOR_CAL2_TEMP               (110L)                       /* Internal temperature sensor, temperature at which temperature sensor has been calibrated in production for data into TEMPSENSOR_CAL2_ADDR (tolerance: +-5 DegC) (unit: DegC). */
#define TEMPSENSOR_CAL_VREFANALOG          (3300UL)                     
1 REPLY 1
SofLit
ST Employee

Almost the same thread: https://community.st.com/t5/stm32-mcus-embedded-software/stm32h743zit6-internal-temperature-sensor-reading/m-p/714636#M50914

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.