cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743XI ADC1 ADC3 DMA data corrupted

XuanXuan
Associate

Hello

I am using  STM32H743XIH6 for Digital Power control. System clock 400MHz. ADC work clock is 36Mhz from pll2 divison. I use a external 36KHz square wave with 50% duty cycle input to GPIO_G11 to trig ADC1 and ADC3 simultaneously to converse regular channel and DMA1 stream0 and DMA1 stream2 to move result to SRAM erea in AXI SRAM.I config ADC1 converse 8 channel spending 160clokcs totally, and ADC3 converse the other 8 channel also 160 clokcs.I read ADC1 and ADC3 sample result data in  DMA1 stream2 converse complete interrupt handler.

ADC1 seventh channel analog input is changed by a analog switch every interrupt.

Also, ADC3 seventh channel analog input is changed by a analog switch every interrupt. Because I controll the external analog switching in every interrupt handle.

I met a problem: my hardware running correct in many many days, but one day ADC1 seventh channel adc converse result I read from sram in interrupt handler is exchange with last data. But ADC3's is always correct.

So, Is there are limit ? ADC3 is fast than ADC1?ADC1 DMA move is slower than read data in interrupt?Is there something do with DSB() instruction?

I also see device errata 2.2.9: Reading from AXI SRAM may lead to data read corruption. Is that the reason? Could you explain? 

This sampling problem cause our High Power three-phase electric product blow up.

We desperately need a explain.Thanks. 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0