2019-05-21 04:50 PM
both ports set to CDC using internal PHY
Heap set to 0x2000
VBus sensing not utilized, but that should only affect 1 port, not both.
using Cube_MX on this new project.
Is there example code for H7 using USB ?
Solved! Go to Solution.
2019-05-21 05:10 PM
Fixed it, the Crystal wasn't running, re-flowed and fixed.
Now Windows recognizes both ports without the use of VBus sensing.
2019-05-21 05:10 PM
Fixed it, the Crystal wasn't running, re-flowed and fixed.
Now Windows recognizes both ports without the use of VBus sensing.
2019-05-21 05:23 PM
Interesting how without a crystal, it doesn't work with the internal RC48 oscillator