2022-11-28 3:40 AM
Dear Forum,
I am using STM32H735 with RTOS LwIP with a DP83826 PHY, and want to see at least a ping on the network.
From HW point of view the PHY seems to work because I can communicate with it and read config registers. The strap pins are set to a valid default configuration.
On the Rx0+Rx1 pins at the uC I can see some incoming frames (oscilloscope), but there are no output Tx0/Tx1 frames visible.
I have checked my configuration against a Nucleo-STM32F439ZI configuration, where a ping works well.
The LWIP_RAM_HEAP_POINTER was configured wrong, but I have set the address in the lwipopts.h file to 0x30004000, so no hard fault anymore.
The function ETH_IRQHandler() is not called event though the NVIC init functions are set:
void HAL_ETH_MspInit(ETH_HandleTypeDef* ethHandle)
{
...
/* Peripheral interrupt init */
HAL_NVIC_SetPriority(ETH_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(ETH_IRQn);
...
}
I did also generate a code sample (just for comparision) with cube with STM32H735 and RTOS and LwIP, but I have no clue where to search or what to check anymore. I have increased the Task Stack a little above the cube-default, but no luck yet.
There is no entry of the MAC in the ARP table of course.
Is there anything else I can check?
2022-11-28 2:35 PM
Hello @MStei.4 ,
Check the PHY parameter for the Ethernet interface.
Is the PHY Address defined in 0?
Imen
2022-11-28 5:38 PM
He said that he can read the PHY registers. And a wrong PHY address will not stop ETH peripheral interrupts from functioning.
2022-11-28 5:40 PM
2022-11-30 1:44 AM
Hello, yes reading / writing PHY registers works fine
DP83826_BMCR: 00003000
DP83826_BMSR: 0000786d
DP83826_PHYIDR1: 00002000
DP83826_PHYIDR2: 0000a111
DP83826_PHYSTS: 00004f11
DP83826_PHYSCR: 0000010b
DP83826_PHYCR: 00008401
The PHY Address is in PHYCR Bit0-4 and is 1, I hope also that I do not have configured something wrong, but the strap pins are setup for basic-mode including RMII interface. rxclk = 50MHz, Bias resistor is correct. 100Mbit is set... all according data sheet. I will investigate in the deadlock that you wrote below, thank you!
2022-11-30 8:57 AM
Maybe my problem is more fundamental. It was a good hint with the tx deadlock, I did the change as described below in the low_level_init but did not help so far.
/* create a binary semaphore used for informing ethernetif of frame reception */
RxPktSemaphore = osSemaphoreNew(1, 0, NULL);
/* create a binary semaphore used for informing ethernetif of frame transmission */
TxPktSemaphore = osSemaphoreNew(1, 0, NULL);
The ETH_IRQHandler() is hit once, I haven't seen it before because of debugging the wrong code part, shame on me. But the error is still the same.
After the IRQHandler hit I press run and pause and then, the heth structure states show that:
gState: 0x23 /*!< an internal process is started */
ErrorCode: 0x08 /*!< DMA transfer error */
DMAErrorCode: 0x4080
I still don't know what is the reason. What else I can chreck here?