2026-04-07 10:54 PM - last edited on 2026-04-08 3:24 AM by mƎALLEm
I am working with the STM32H723ZG and trying to implement Ethernet communication without using an RTOS using LWIP(TCP/IP)
Setup Details:
Board: NUCLEO-H723ZG
IDE: STM32CubeIDE v1.19.0
Ethernet stack: LwIP
PHY interface: RMII
Flashing tool: ST-LINK (onboard)
Test performed: Ping test from PC
Observed behavior:
The Ethernet port LEDs (orange and green) remain solid ON after connecting the Ethernet cable.
Ping is failing continuously, I got (Destination host unreachable) error.
Troubleshoot taken:
Checked with multiple Ethernet cables to ensure cable isn't a problem.
Rebuilt and reflashed the project multiple times.
After all this still I can't ping the board.
Assistance required :
I'm providing my Project file below
Any guidance or working minimal examples for STM32H7 Ethernet (without RTOS) would be greatly appreciated.
2026-04-13 8:34 AM
Hello again,
I believe I found the issue preventing your application from working.
The names of the memory sections dedicated to the descriptors in the linker file do not match those declared in ethernetif.c. In ethernetif.c, the section names are RxDescripSection and TxDescripSection (with an “s”):
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDescripSection"))); /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDescripSection"))); /* Ethernet Tx DMA Descriptors */
However, in your linker file, the sections are declared as RxDecripSection and TxDecripSection (without the “s”). Below, you will find a fixed version of the project that has been tested and works.
Best regards,
2026-04-16 8:25 AM
Hello @STackPointer64 ,
Sorry for the delayed reply. I flashed the file you given it works good at first but if I rebuild it and flash it again, it is not pinging, some file is not generating while I rebuild it and in the first time flashing it is not working after the power cycle.
please check with the last updated project file and let me know what's the issue.
Thank you,
2026-04-17 8:28 AM
Hello @max67,
That is rather unusual, as I tested the project and it worked before I sent it. Have you tried opening the project in a new STM32CubeIDE workspace? Could you try rebuilding the attached project, make sure that it does not work, compress it, and attach it to this thread so I can compare what changed between compilations? Also, try inspecting the network traffic using Wireshark when the board is plugged in to see whether an ARP announcement is being sent. Try changing the IP address and rebuilding to see if it is related to a network policy issue.
Best regards,
2026-04-17 9:58 AM
> and in the first time flashing it is not working after the power cycle.
Hmm.. this hints to the PHY reset issue?
2026-05-07 1:36 AM
Hi, @Pavel A. and @STackPointer64
I'm having the same issue as @max67. Same setup, except the CubeIDE version is 2.1.1. I have downloaded the ETHERNET_H723_fixed.zip that STackPointer64 uploaded. First built and ran it without any changes, connected the STM to my PC's ethernet port, ping failed ("Destination host unreachable"). Then I connected PC and STM to my router, changed the IP to match my router setup, ping still fails. I don't think this is a network policy issue, because the same setup works for my Pico W5500-EVB.
I have tried many examples, including https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308/show-comments/true and the related project from GitHub. Nothing works.
I have attached the project I built with new IP. Any help is appreciated, thanks.
2026-05-07 4:58 AM
Hello @max67 ,
Currently im also facing the same issue that your have faced , did you found a solution for it, if yes kindly share the solution and Help me how to rectify it, ill add my code to you