STM32H723VE Ethernet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-21 5:12 AM
Hello,
I'm using the STM32H723VE chip in my project and I'm having some difficulties getting the Ethernet interface fully functional. Used this chip with the KSZ8041 and I'm giving ping. I enabled the D-Cache and I-Cache, performed the MPU settings. I'm trying to implement the Modbus TCP protocol, I open and close the TCP connection, it works for a while and then it stops working and then it doesn't work anymore. I'm a few things on the forum, however nothing has yet worked.
I use STM32Cube FW_H7 V1.11.0 (6.8.0).
Some relevant settings:
**** __FLASH.id
/* Modification start */
.lwip_sec (NOLOAD) : {
. = ABSOLUTE(0x30000000);
*(.RxDecripSection)
. = ABSOLUTE(0x30000080);
*(.TxDecripSection)
. = ABSOLUTE(0x30000100);
*(.Rx_PoolSection)
} >RAM_D2
/* Modification end */
**** lwipopts.h
/* STM32CubeMX Specific Parameters (not defined in opt.h) ---------------------*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- WITH_RTOS enabled (Since FREERTOS is set) -----*/
#define WITH_RTOS 1
/* Temporary workaround to avoid conflict on errno defined in STM32CubeIDE and lwip sys_arch.c errno */
#undef LWIP_PROVIDE_ERRNO
#define LWIP_ERRNO_STDINCLUDE
/*----- WITH_MBEDTLS enabled (Since MBEDTLS and FREERTOS are set) -----*/
#define WITH_MBEDTLS 0
/*----- CHECKSUM_BY_HARDWARE enabled -----*/
#define CHECKSUM_BY_HARDWARE 0
/*-----------------------------------------------------------------------------*/
/* LwIP Stack Parameters (modified compared to initialization value in opt.h) -*/
/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/
/*----- Value in opt.h for LWIP_DHCP: 0 -----*/
#define LWIP_DHCP 1
/*----- Default value in ETH configuration GUI in CubeMx: 1524 -----*/
#define ETH_RX_BUFFER_SIZE 1536
/*----- Value in opt.h for LWIP_DNS: 0 -----*/
#define LWIP_DNS 0
/*----- Default Value for MEMP_NUM_UDP_PCB: 4 ---*/
#define MEMP_NUM_UDP_PCB 6
/*----- Default Value for MEMP_NUM_TCP_PCB: 5 ---*/
#define MEMP_NUM_TCP_PCB 8
/*----- Value in opt.h for MEM_ALIGNMENT: 1 -----*/
#define MEM_ALIGNMENT 4
/*----- Default Value for MEMP_NUM_NETCONN: 4 ---*/
#define MEMP_NUM_NETCONN 16
/*----- Default Value for MEM_SIZE: 1600 ---*/
#define MEM_SIZE 4*1024
/*----- Default Value for H7 devices: 0x30044000 -----*/
#define LWIP_RAM_HEAP_POINTER 0x30002000
/*----- Value supported for H7 devices: 1 -----*/
#define LWIP_SUPPORT_CUSTOM_PBUF 1
/*----- Value in opt.h for LWIP_ETHERNET: LWIP_ARP || PPPOE_SUPPORT -*/
#define LWIP_ETHERNET 1
/*----- Default Value for LWIP_RANDOMIZE_INITIAL_LOCAL_PORTS: 0 ---*/
#define LWIP_RANDOMIZE_INITIAL_LOCAL_PORTS 1
/*----- Default Value for LWIP_MULTICAST_TX_OPTIONS: 0 ---*/
#define LWIP_MULTICAST_TX_OPTIONS 1
/*----- Default Value for LWIP_DHCP_CHECK_LINK_UP: 0 ---*/
#define LWIP_DHCP_CHECK_LINK_UP 1
/*----- Value in opt.h for LWIP_DNS_SECURE: (LWIP_DNS_SECURE_RAND_XID | LWIP_DNS_SECURE_NO_MULTIPLE_OUTSTANDING | LWIP_DNS_SECURE_RAND_SRC_PORT) -*/
#define LWIP_DNS_SECURE 7
/*----- Default Value for TCP_MSS: 536 ---*/
#define TCP_MSS 1460
/*----- Value in opt.h for TCP_SND_QUEUELEN: (4*TCP_SND_BUF + (TCP_MSS - 1))/TCP_MSS -----*/
#define TCP_SND_QUEUELEN 9
/*----- Value in opt.h for TCP_SNDQUEUELOWAT: LWIP_MAX(TCP_SND_QUEUELEN)/2, 5) -*/
#define TCP_SNDQUEUELOWAT 5
/*----- Default Value for LWIP_NETIF_API: 0 ---*/
#define LWIP_NETIF_API 1
/*----- Default Value for LWIP_NETIF_STATUS_CALLBACK: 0 ---*/
#define LWIP_NETIF_STATUS_CALLBACK 1
/*----- Value in opt.h for LWIP_NETIF_LINK_CALLBACK: 0 -----*/
#define LWIP_NETIF_LINK_CALLBACK 1
/*----- Default Value for LWIP_NETIF_STATUS_CALLBACK: 0 ---*/
#define LWIP_NETIF_STATUS_CALLBACK 1
/*----- Value in opt.h for TCPIP_THREAD_STACKSIZE: 0 -----*/
#define TCPIP_THREAD_STACKSIZE 1024
/*----- Value in opt.h for TCPIP_THREAD_PRIO: 1 -----*/
#define TCPIP_THREAD_PRIO 24
/*----- Value in opt.h for TCPIP_MBOX_SIZE: 0 -----*/
#define TCPIP_MBOX_SIZE 6
/*----- Value in opt.h for SLIPIF_THREAD_STACKSIZE: 0 -----*/
#define SLIPIF_THREAD_STACKSIZE 1024
/*----- Value in opt.h for SLIPIF_THREAD_PRIO: 1 -----*/
#define SLIPIF_THREAD_PRIO 3
/*----- Value in opt.h for DEFAULT_THREAD_STACKSIZE: 0 -----*/
#define DEFAULT_THREAD_STACKSIZE 1024
/*----- Value in opt.h for DEFAULT_THREAD_PRIO: 1 -----*/
#define DEFAULT_THREAD_PRIO 3
/*----- Value in opt.h for DEFAULT_UDP_RECVMBOX_SIZE: 0 -----*/
#define DEFAULT_UDP_RECVMBOX_SIZE 6
/*----- Value in opt.h for DEFAULT_TCP_RECVMBOX_SIZE: 0 -----*/
#define DEFAULT_TCP_RECVMBOX_SIZE 6
/*----- Value in opt.h for DEFAULT_ACCEPTMBOX_SIZE: 0 -----*/
#define DEFAULT_ACCEPTMBOX_SIZE 6
/*----- Default Value for LWIP_SO_RCVTIMEO: 0 ---*/
#define LWIP_SO_RCVTIMEO 1
/*----- Value in opt.h for RECV_BUFSIZE_DEFAULT: INT_MAX -----*/
#define RECV_BUFSIZE_DEFAULT 2000000000
/*----- Value in opt.h for LWIP_USE_EXTERNAL_MBEDTLS: 0 -----*/
#define LWIP_USE_EXTERNAL_MBEDTLS 0
/*----- Default Value for LWIP_HTTPD: 0 ---*/
#define LWIP_HTTPD 0
/*----- Value in opt.h for HTTPD_USE_CUSTOM_FSDATA: 0 -----*/
#define HTTPD_USE_CUSTOM_FSDATA 0
/*----- Default Value for LWIP_SNTP: 0 ---*/
#define LWIP_SNTP 0
/*----- Default Value for LWIP_TFTP: 0 ---*/
#define LWIP_TFTP 0
/*----- Default Value for LWIP_STATS: 0 ---*/
#define LWIP_STATS 1
/*----- Value in opt.h for MIB2_STATS: 0 or SNMP_LWIP_MIB2 -----*/
#define MIB2_STATS 0
/*----- Value in opt.h for CHECKSUM_GEN_IP: 1 -----*/
#define CHECKSUM_GEN_IP 0
/*----- Value in opt.h for CHECKSUM_GEN_UDP: 1 -----*/
#define CHECKSUM_GEN_UDP 0
/*----- Value in opt.h for CHECKSUM_GEN_TCP: 1 -----*/
#define CHECKSUM_GEN_TCP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP: 1 -----*/
#define CHECKSUM_GEN_ICMP 0
/*----- Value in opt.h for CHECKSUM_GEN_ICMP6: 1 -----*/
#define CHECKSUM_GEN_ICMP6 0
/*----- Value in opt.h for CHECKSUM_CHECK_IP: 1 -----*/
#define CHECKSUM_CHECK_IP 0
/*----- Value in opt.h for CHECKSUM_CHECK_UDP: 1 -----*/
#define CHECKSUM_CHECK_UDP 0
/*----- Value in opt.h for CHECKSUM_CHECK_TCP: 1 -----*/
#define CHECKSUM_CHECK_TCP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP: 1 -----*/
#define CHECKSUM_CHECK_ICMP 0
/*----- Value in opt.h for CHECKSUM_CHECK_ICMP6: 1 -----*/
#define CHECKSUM_CHECK_ICMP6 0
RX_POOL is coming in RAM_D2.
- Labels:
-
Ethernet
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-22 12:30 AM
Hello @GTrin.2​ ​ and welcome to the Community :),
Please follow this article "Ethernet not working on STM32H7x3", it may resolve your problem.
Also, I advise you, when you configurated the ethernet project, to get inspired form the steps described in this FAQ: How to create project for STM32H7 with Ethernet and LwIP stack working.
This FAQ will help you to configure your project in STM32CubeMX .
Also, you can get started with the example provided here STM32H7-LwIP-Examples.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-03-22 9:56 AM