cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 USB-DFU Not Working

EPala.2
Associate III

Hi, I am working on a project where we need USB DFU on the STM32H730. I have selected the USB DFU function in the .IOC, compiled and uploaded to the hardware, but when I try uploading a new program both via this online DFU Tester (https://devanlai.github.io/webdfu/dfu-util/) and via CubeProgrammer in USB DFU mode. Neither works. I have attached some screenshots of my .IOC settings and of the errors I am getting.

How do I fix this?

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

DFU in ioc is i mean for implement your own protocols and code. Set it in ioc do only prepare phase, no ready design.

For load firmware use sytem code STM32 microcontroller system memory boot mode - Application note

View solution in original post

1 REPLY 1
MM..1
Chief III

DFU in ioc is i mean for implement your own protocols and code. Set it in ioc do only prepare phase, no ready design.

For load firmware use sytem code STM32 microcontroller system memory boot mode - Application note