cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0B1 USB-PD

DDeba.1
Associate III

Hi, 

I am using the STM32G0B1CBTX with STM32CubeMX ver 6.13.0 to produce a USB-PD DRP application. So far, I managed to implement a USB 2.0 Host as this is also needed. When trying to add the USB-PD DRP following ST-s tutorial BUT omitting the inclusion of the OS, I get a hard fault immediately after running the firmware. Moreover, I need to use the USB-PD library without the OS.

1. I tried to check what is causing the hard fault but I cannot find any documentation on how to view the hard fault status or any reference to hard fault registers. Can someone point me to any documentation. 

2. Are there any references on how to implement the USB-PD with out the use of an OS?

 

Thanks

0 REPLIES 0