cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F756BGT6: Embedded Bootloader

vgiampa
Associate

Dear Sir/Madam,

I have two question to better understand the Embedded bootloader of the STM32F7 Microcontroller and relevant configuration with respect to the Silicon Revision.

  1. Is it possible to perform an overwrite of the embedded bootloader programmed by ST Microelectronics during production in the system memory?
  2. If the Embedded Bootloader change version (i.e. from v9.0 to 9.1) the relevant silicon revision of the microcontroller shall be updated or not? Is it possible to know from the silicon revision of STM32 P/N which is the relevant embedded bootloader version?

I am looking forward to receive your feedback,

Best Regards

Valerio Giampà

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @vgiampa​, to the community!

  1. no, the embedded bootloader is fixed and cannot be overwritten
  2. the embedded boot loader version can be obtained using the get command in case you need to know it

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

ST writes the System Loader firmware, it is not etched, and is independent of the chip revision/stepping.

Consider it as using OTP memory.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..