2020-02-20 5:03 PM
I'm trying to use FreeRTOS to write ADC data to SD card on the STM32F7 and I'm using V1 of the CMSIS-RTOS API.
I'm trying to use mail queues and I have a struct that holds an array.
typedef struct
{
uint16_t data[2048];
} ADC_DATA;on the ADC half/Full complete interrupts, I add the data to the queue and I have a consumer task that writes this data to the sd card. My issue is in my Consumer Task, I have to do a memcpy to another array and then write the contents of that array to the sd card
void vConsumer(void const * argument)
{
ADC_DATA *rx_data;
for(;;)
{
writeEvent = osMailGet(adcDataMailId, osWaitForever);
if(writeEvent.status == osEventMail)
{
// write Data to SD
rx_data = writeEvent.value.p;
memcpy(sd_buff, rx_data->data, sizeof(sd_buff));
if(wav_write_result == FR_OK)
{
if( f_write(&wavFile, (uint8_t *)sd_buff, SD_WRITE_BUF_SIZE, (void*)&bytes_written) == FR_OK)
{
file_size+=bytes_written;
}
}
osMailFree(adcDataMailId, rx_data);
}
}This works as intended but if I try to change this line to
f_write(&wavFile, (uint8_t *)rx_data->data, SD_WRITE_BUF_SIZE, (void*)&bytes_written) == FR_OK)f_write returns FR_DISK_ERR. Can anyone help shine a light on why this happens, I feel like the extra memcpy is useless and you should just be able to pass the pointer to the queue straight to f_write.
2020-02-20 6:43 PM
DMA would have memory alignment and memory region dependencies.
Watch for cache coherency issues.
Perhaps look at the addresses in failing, vs non-failing cases.