cancel
Showing results for 
Search instead for 
Did you mean: 

Data exchange via USB interface (CDC protocol) between Nucleo Board L4 and a PC. Unfortunately the USB interface does not work. What can I do to use the virtual COM port?

MScha.1
Associate II

I want to send data with a data rate of about 5Mbit/s from my Nucleo L476RG board to Matlab using the USB interface with the CDC protocol.

For the USB connection I need to have 48MHz USB clock. I soldered a 8MHz / 16pF crystal at position X3 on the board and assembled C33 / C34 with 20 pF capacitors. In the Clock configuration I specified an external 8MHz source and set the USB clock to 48MHz. A blinking LED program shows me that the clock is correct.

But I am not able to use the port. What am I doing wrong?

For your information:

I use the Nucleo L476RG board. The PC runs with Windows 10.

The tool chain used is:

CubeMX 5.5.0 and SW4STM32 version Neon.3 release 4.6.3.

USB is connected as follows:

GND connected to Nucleo

VCC (+5V) not connected

D+ via a 1.5k pull up resistor to 3.3V and connected to PA12

D- connected with PA11

In CubeMX the following is set:

Connectivity:

USB_OTG_FS / Device_Only

"Activate_SOF" and "Activate_VBUS" are inactive.

Middleware: USB_Device / Communication Device Class (Virtual Port Com)

In the Project I increased the minimum heap size from 0x100 to 0x800.

In the main.c program the following 3 additions are made:

1)

/* Private includes --------*/

/* USER CODE BEGIN Includes */

#include "usbd_cdc_if.h"

2)

/* USER CODE BEGIN 2 */

 HAL_Delay(1000);

 uint8_t buffer[] = "Hallo, Welt!\r\n";

3)

 /* USER CODE BEGIN WHILE */

 while (1)

 {

    CDC_Transmit_FS(buffer, sizeof(buffer));

    HAL_Delay(1000);

    HAL_GPIO_TogglePin(LD2_GPIO_Port,LD2_Pin);

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0