cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429ZI FATFS issue

zeboss49
Associate III

Hello,

I'm trying to use FatFS with both USB HOST MSC class and SDIO.

FatFS always tries to access the SD card whatever the drive number used in f_mount.

May be I'm wrong with the path I use to access the devices : "0" for SD card, "1" for USB.

Any help will be welcome.

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Issue is solved.

I stepped into f_mount and found thaht the path was missing the ":" i.e. path must be "0:" or "1:" not bjust "0" or "1".

Thanks for the answer :)

 

 

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @zeboss49 

Can you add your code to understand more about your request.

Best regards.

II

Issue is solved.

I stepped into f_mount and found thaht the path was missing the ":" i.e. path must be "0:" or "1:" not bjust "0" or "1".

Thanks for the answer :)