2017-11-02 10:40 AM
Hey Guys,
I am setting up some STM32F407VETx on a chinese breakout board with �SD-card-slot.
I try to read data from the sd card with SDIO (SD 4 bits Wide bus) and FatFs.
The Basic-Project is build with STM32 CubeMx and programmed in the OpenSTM32 Workbench.
My Problem:
The SD Card is ALWAYS in 'FR_NOT_READY'. I am not able to mount / open / write any data, because the �C is always stuck in the following function:
/**
* @brief Checks for error conditions for R1 response. * @param hsd SD handle * @param SD_CMD The sent command index * @retval SD Card error state */static uint32_t SDMMC_GetCmdResp1(SDIO_TypeDef *SDIOx, uint8_t SD_CMD, uint32_t Timeout){...
}
Because of the timeout in this function i get an errorcode '1' (R/W Error ) in diskio.c
I've tried 3 boards, 3 SD-cards - nothing is broken! I have no clue, what to do...
I am just using the 'basic' fatfs functions, as you can the in the attachment.
Please help me!
:(
Greets!
Ps.: If you need more information, please write some comment!
#sdio #error #sd #stm32f407 #sd-card #fatfs2017-12-01 6:07 PM
Hi Haithem,
I found this post and found the issue, I also posted it to the main forum. Please see:
https://community.st.com/0D50X00009XkXg5SAF
It seems that the write and read interrupt and dma functions had state errors.
Regards,
Piet
2017-12-07 1:13 AM
Hello,
Please refer to
https://community.st.com/0D50X00009bMM8bSAG
andhttps://community.st.com/0D50X00009XkXg5SAF
if you face similar issue at your end.-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.