cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405 CDC USB isn't enumerated by the host

Jcoll.1
Associate III

I have a new STM32F405 based board design. It is USB powered. In cube IDE I have the STM USB section configured as 'device only', 'no vbus sensing', and I have the middleware set to CDC and 'USBD_SELF_POWERED' is disabled (although I have tried both settings).

When I plug the board in to a host the host wont even attempt to enumerate it. I have also checked this with wireshark. I have tried several known-good cables and USB ports. The fact that the host won't try to enumerate makes me think that the STM is not pulling the D+ pin high.

As a test I powered the board from a bench supply, with no USB cable attached, and measured the D+ and D- pins. I expected to see 3.3V on D+ but instead I see about 500mV on each pin. This is suspiciously close to a diode breakdown voltage, so I double checked the orientation of my USB ESD package and it appears to be correct.

Before I remove this package, does anyone have any suggestions for things I can test in hardware or software?

EDIT #1 - I removed the ESD chip and D+ and D- continue to float around 500mV (when not attached to a host) and the host does not attempt to enumerate.

EDIT #2 - The chip is STM32F405VGT6. I believe this chip has integrated USB pull-up resistors.

6 REPLIES 6

IF OTG_FS, DFU bootloader enumerates?

JW

Thanks for your reply, JW.

I don't know what "IF OTG_FS" means.

I've never used the USB bootloader, but my understanding is that if I pull BOOT0 high that it should allow programming via USB. I just tried this and it clearly does not load my default program, however I also don't see any USB activity.

I went ahead and removed the ESD protection chip and confirmed the pinout from the end of a USB cable to the chip.

I still do not see an enumeration attempt from the PC, even when pulling BOOT0 high. And more importantly, when running my application, D+ and D- continue to float around 500mV (when not attached to host).

Is VUSB required for the bootloader to work?

I meant, you can test the hardware through bootloader, if the USB you are using is OTG_FS, as bootloader uses only that (and if you use a crystal with integer values as outlined by AN2606).

In other words, which pins are you using?

If DP is not pulled up, check if DP/DM are properly set in GPIO by reading out and checking the respective GPIO registers; then check if the USB module has clock set in the respective enable register in RCC, then check the OTG registers - you should have GCCFG.NOVBUSSENS = 1, GCCFG.PWRDWN = 1, DCTL.SDIS = 0.

I don't use Cube so can't help with that.

JW

Ah, I understand now. Looking at AN2606 my setup should support USB DFU (16MHz clock; PA11 and PA12, the OTG_FS pins). BUT, since I wasn't planning to use this feature I didn't route the BOOT1 pin, which is required to get into the bootloader (BOOT1=0, BOOT0=1). I ran out of fine gauge wire to manually jumper that, so I won't be able to try the USB DFU until Saturday.

I ended up finding the problem. My clock configuration had the system clock being sourced from HSI while USB (the 48MHz clock?) was being sourced through the PLL by the HSE. I found that if I sourced the entire design from HSE that the system would fail. On closer inspection the HSE is never going ready. Specifically this line is never passed: `while(__HAL_RCC_GET_FLAG(RCC_FLAG_HSERDY) == RESET)`. I can get around this problem by sourcing the PLL from the HSI.

I suppose I should start a new thread to troubleshoot the HSE issue. The parts and design come from a known working project, so I'm thinking maybe an assembly error.

HSI is not precise enough to run USB. There is also some minimum system clock frequency requirement for USB to work (14MHz IIRC).

JW