2021-03-17 7:10 AM
Hello,
I am able run successfully mqtt example on my stm32f4 MCU and on my local network.
I want to run the same code on a cloud platform. However there is a link provided by mqtt cloud provider not an IP address like 192.168.0.10
Can I directly use the below link instead of the IP address ? If not, then How can I ?
1f87a053302042c7a0ccb2dac5d1263b.s1.eu.hivemq.cloud
Best Regards
Solved! Go to Solution.
2022-08-25 10:45 PM
Hello @voyvoda .,
I tried to connect to MQTT server using LWIP protocol from STM32F4. I am able to connect but getting authentication failure in MQTT server side. And, not able to publish the date to the server. Kindly help resolve this issue.
2024-04-02 5:39 AM
Good day
Have you been able to solve the problem? I know it is a long time ago, but any possibility of code sharing?
Or even a link to working software. I am using the STM32H563Z