cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with mbedtls_x509_crt_parse on STM32F407 using LWIP and MQTT for Azure IoT Hub

Noushadalik
Associate III

Hello STM Community,

I am currently working on a project using an STM32F407 microcontroller with LWIP and MQTT to connect to Azure IoT Hub on the secure MQTT port 8883. I am encountering an issue with the mbedtls_x509_crt_parse function when trying to create a TLS configuration. The error message I receive is

 

mbedtls_x509_crt_parse ca failed: -15104 0x3b00 Failed to create TLS configuration.

 

Code Snippet:

 

const char azure_root_ca[] = "-----BEGIN CERTIFICATE-----\r\n" "MIIDjjCCAnagAwIBAgIQAzrx5qcRqaC7KGSxHQn65TANBgkqhkiG9w0BAQsFADBh\r\n" "MQswCQYDVQQGEwJVUzEVMBMGA1UEChMMRGlnaUNlcnQgSW5jMRkwFwYDVQQLExB3\r\n" "d3cuZGlnaWNlcnQuY29tMSAwHgYDVQQDExdEaWdpQ2VydCBHbG9iYWwgUm9vdCBH\r\n" "MjAeFw0xMzA4MDExMjAwMDBaFw0zODAxMTUxMjAwMDBaMGExCzAJBgNVBAYTAlVT\r\n" "MRUwEwYDVQQKEwxEaWdpQ2VydCBJbmMxGTAXBgNVBAsTEHd3dy5kaWdpY2VydC5j\r\n" "b20xIDAeBgNVBAMTF0RpZ2lDZXJ0IEdsb2JhbCBSb290IEcyMIIBIjANBgkqhkiG\r\n" "9w0BAQEFAAOCAQ8AMIIBCgKCAQEAuzfNNNx7a8myaJCtSnX/RrohCgiN9RlUyfuI\r\n" "2/Ou8jqJkTx65qsGGmvPrC3oXgkkRLpimn7Wo6h+4FR1IAWsULecYxpsMNzaHxmx\r\n" "1x7e/dfgy5SDN67sH0NO3Xss0r0upS/kqbitOtSZpLYl6ZtrAGCSYP9PIUkY92eQ\r\n" "q2EGnI/yuum06ZIya7XzV+hdG82MHauVBJVJ8zUtluNJbd134/tJS7SsVQepj5Wz\r\n" "tCO7TG1F8PapspUwtP1MVYwnSlcUfIKdzXOS0xZKBgyMUNGPHgm+F6HmIcr9g+UQ\r\n" "vIOlCsRnKPZzFBQ9RnbDhxSJITRNrw9FDKZJobq7nMWxM4MphQIDAQABo0IwQDAP\r\n" "BgNVHRMBAf8EBTADAQH/MA4GA1UdDwEB/wQEAwIBhjAdBgNVHQ4EFgQUTiJUIBiV\r\n" "5uNu5g/6+rkS7QYXjzkwDQYJKoZIhvcNAQELBQADggEBAGBnKJRvDkhj6zHd6mcY\r\n" "1Yl9PMWLSn/pvtsrF9+wX3N3KjITOYFnQoQj8kVnNeyIv/iPsGEMNKSuIEyExtv4\r\n" "NeF22d+mQrvHRAiGfzZ0JFrabA0UWTW98kndth/Jsw1HKj2ZL7tcu7XUIOGZX1NG\r\n" "Fdtom/DzMNU+MeKNhJ7jitralj41E6Vf8PlwUHBHQRFXGU7Aj64GxJUTFy8bJZ91\r\n" "8rGOmaFvE7FBcf6IKshPECBV1/MUReXgRPTqh5Uykw7+U0b6LJ3/iyK5S9kJRaTe\r\n" "pLiaWN0bfVKfjllDiIGknibVb63dDcY3fe0Dkhvld1927jyNxF1WW6LZZm6zNTfl\r\n" "MrY=\r\n" "-----END CERTIFICATE-----\r\n"; struct altcp_tls_config *tls_config; const size_t mbedtls_root_certificate_len = strlen(azure_root_ca); tls_config = altcp_tls_create_config_client((const u8_t*)azure_root_ca, mbedtls_root_certificate_len); if (tls_config == NULL) { printf("Failed to create TLS configuration.\n"); return; }

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Noushadalik
Associate III

Hello,
The mbedtls_x509_crt_parse CA failed with error -15104 (0x3b00). I resolved this issue by changing the size of "MBEDTLS_MPI_MAX_SIZE."

 

View solution in original post

1 REPLY 1
Noushadalik
Associate III

Hello,
The mbedtls_x509_crt_parse CA failed with error -15104 (0x3b00). I resolved this issue by changing the size of "MBEDTLS_MPI_MAX_SIZE."