STM32f4 discorvery, fatfs, SD card problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-29 6:54 AM
Hi all,
I'm working on getting a discovery board working with an SD card. I'm using CubeMx v4.25.0 with package v1.21.0.
Hardware connection is validated and is correct.
I run into a problem when I try to open a file. A
FR_DISK_ERR error is returned.
The error looks like the problem mentioned in:
https://community.st.com/0D50X00009XkX55SAF
The error seems to come from this line:
if (disk_read(fs->drv, fs->win.d8, sector, 1) != RES_OK) in ff.c
Possible fixes mentioned in the linked post do not work.
Any clues about this?
#fatfs #sd-card #stm32f4-discovery #sdio- Labels:
-
FatFS
-
SDIO-SDMMC
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-29 9:17 AM
>>
Any clues about this?
You'll need to dig below this, the underlying read to the SD card is failing, presumably in sd_diskio.c, you'd want to instrument that.
There is workable code for the SD cards under the HAL example trees if CubeMX doesn't work.
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
‎2018-04-25 5:40 AM
Hi,
I exactly have the same problem. In fact, I traced down to the same line as stated.
Besides, I've managed to make it work with CubeMX v4.21 with FW v1.16, however I cannot make it work with CubeMX v4.25 with FW v1.21 (current latest version).
I tried the solution provided in here:
https://community.st.com/0D50X00009bMM8bSAG
This did not solve my problem.
Looking forward to hear any workaround as soon as possible, and ultimately a fix in the next version.
Regards,
Ogulcan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-25 8:13 AM
You're going to need to trace it deeper to understand why the sector read isn't working.
Should perhaps not be dependent on CubeMX, but rather look at the SD/FatFs examples with HAL. At the very least use the examples to test your interface and card functionality under 1.21
ST has let this mess drag on far too long...
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
‎2018-04-25 9:02 AM
Hi Clive,
I have managed to make my hardware work with CubeMX version 4.21 and F4 FW version 1.16, so I know that there is no hardware issue. I followed this video to do so:
https://www.youtube.com/watch?v=0NbBem8U80Y
I tried the HAL examples beforehand given in STM32Cube_FW_F4_V1.21.0, but STM32F4 Discovery Board does not have uSD example as the board does not have uSD without its base board. I've copied from others and those did not work.
I also cannot downgrade my original project as CubeMX does not let me to do so. Therefore, I'll most probably skip this task until a new fixed version is released.
Regards,
Ogulcan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-25 10:34 AM
With the exception of the GPIO pin chosen for Card Detect functionality the SDIO/SDMMC pins are quite strongly defined across a range of F4 products. I tend to build to the STM32F4DIS-BB schematic as I have a bunch of those.
The NUCLEO-144 has turned into my break-out board of preference these days. Have a bunch of working SDIO/SDMMC projects for those across most families.
Up vote any posts that you find helpful, it shows what's working..