2022-11-24 11:58 PM
Hi,
I studied the RM0091 (page 55). There UART, I2C is listed as supported interfaces for the internal bootloader.
I was wondering why the CAN isn't supported. Is this the case?
Thanks
Solved! Go to Solution.
2022-11-25 12:18 AM
Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.
Does it answer your question?
Regards
/Peter
2022-11-25 12:18 AM
Correct, AN2606 lists all possible interfaces for the various STM32s, but there is no family with bootloader via CAN for the STM32F0 yet.
Does it answer your question?
Regards
/Peter
2022-11-25 12:40 AM
Yes, it does.
Thank you for the prompt answer.
2022-11-25 12:44 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2022-11-25 1:08 AM
Before you happily jump into using the STM canbus bootloader, have it mind it WONT WORK if more than one canbus node is active.
I realiced it the hard way https://community.st.com/s/question/0D53W00000apgoISAQ/is-the-stm-system-bootloader-trough-canbus-just-not-woking-when-more-than-one-device-shares-the-bus