2021-07-01 6:52 AM
Hi all,
First some context:
I am attempting to use the USB designated pins (PA11 and PA12) as generic GPIO inputs at start-up as a way of determining if a host is connected to the device and make a decision whether to run the main code or not - I will have external pull-up resistors on the DP and DM lines to aid this. Whilst waiting for the board to be made I wanted to make sure I could read the pin levels at start-up - for this I used the STM32F0-Discovery board.
This is where I encountered my issue. I initially tried setting pins PA11 and PA12 as inputs with a pull-up resistor, I would then use a 'flying wire' to alternate the pin voltage between 0V and 5V. I then set up the code such that the LEDs would change state depending on the input pins. The code can be seen here:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2021 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_WritePin(LED_USB_GPIO_Port, LED_USB_Pin, HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_11));
HAL_GPIO_WritePin(LED_AXIOM_GPIO_Port, LED_AXIOM_Pin, HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_12));
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, LED_USB_Pin|LED_AXIOM_Pin, GPIO_PIN_RESET);
/*Configure GPIO pins : LED_USB_Pin LED_AXIOM_Pin */
GPIO_InitStruct.Pin = LED_USB_Pin|LED_AXIOM_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11|GPIO_PIN_12, GPIO_PIN_SET);
/*Configure GPIO pin : PA11 */
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PA12 */
GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(char *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
No matter what voltage/logic level I applied to the pins the LEDs did not change state.
I then set PA11 and PA12 as output push-pulls, made them write high, and used a logic analyser to scope the pins. With this set-up the pins should have been outputting a logic 1, however they remained at 0!
In short, I do not seem to be able to use these pins as regular GPIOs. I have tried looking through the documentation for any reference to this behaviour but came up with nothing. I know it is not how I am setting the pins up as applying the same process/config to PA9 and PA10 yields the expected results.
Any ideas?
James
Solved! Go to Solution.
2021-07-02 7:42 AM
Hi TDK,
> IDR following the pull resistor but not your input would suggest you're not applying the input to the pin. Where exactly are you applying the flying pin?
That would be my assumption as well. It almost seems as though the pin on the board isn't physically connected to the chip. I have a lead connecting PA11 to GND on the discovery board as shown in the photo.
2021-07-02 7:49 AM
> It almost seems as though the pin on the board isn't physically connected to the chip.
By default, it isn't.
JW
2021-07-02 8:27 AM
Ah that would explain a lot. Thanks a lot for your help, I should've looked at that document a lot earlier. I'll join that bridge and report back whether it springs back to life (which I am very certain it will).
2021-07-02 9:06 AM
> STM32F0-Discovery board
I checked the schematic beforehand and it did not show these solder bridges.
Turns out the issue was that I was looking at STM32F0-DISCOVERY board (per the OP), whereas the OP actually had the 32F072BDISCOVERY board, despite it saying "stm32f0-discovery" on the board itself. The OP also says STM32F072xB so can't really fault.
https://www.st.com/en/evaluation-tools/stm32f0discovery.html
vs
https://www.st.com/en/evaluation-tools/32f072bdiscovery.html
2021-07-02 11:53 AM
You can because I've already asked :)
JW
2021-07-05 3:09 AM
I have joined those bridges and now have the expected behaviour, thank you both for your help it is greatly appreciated.
Apologies for any unnecessary confusion I caused, I was not aware there were 2 evaluation boards (with a similar name) and somehow didn't notice that even with the page JW linked - that'll teach me to take a bit more time reading next time.
James