STM32F0 Scan ADC Polling Sequence
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-11 12:41 AM
Good Day
Please help me understand if I am using the Polling Mode correctly for the ADC. I have not gone through the trouble of setting up DMA or Interrupts because these functions will hardly ever be used in my system.
I have set up the ADC to convert 4 Channels for me, Channel 1, Channel5, VREFINT and Temperature sensor, like this:
void MX_ADC_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = DISABLE; //AJ 10Apr changed from ENabled
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/**Configure for the selected ADC regular channel to be converted. */
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; // See AN3116
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_VREFINT;/* Get 3V3 Volt reading from this */
sConfig.Rank = 2;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_5; /* 5V Div to 2.5V */
sConfig.Rank = 3;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
sConfig.Rank = 4;
sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
HAL_ADCEx_Calibration_Start(&hadc); // Calibrate
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
After starting the ADC, it is my understanding that I need to Poll for a conversion and then go and read the result, which will be the result for Rank1, and then poll again and read the result, which should be Rank 2, and poll again and read and the result should be for Rank3, and then poll one more time to read the result for Rank 4, and then callingto stop the ADC. Next time I start it, it will restart from Rank1. Is this correct? I am not getting the expected values for Ranks 2, 3 and 4, though the result for Rank1 seems to be correct.
HAL_ADC_Start(&hadc);
uint16_t ADCValue = 0x00;
uint16_t MCUTemperatureDegrees = 0;
if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) == HAL_OK)
{
ADCValue = HAL_ADC_GetValue(&hadc); /* Gets CH1 */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue = HAL_ADC_GetValue(&hadc); /* Gets 3V3 */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue = HAL_ADC_GetValue(&hadc); /* Gets 5V */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue = HAL_ADC_GetValue(&hadc); /* Gets Temp */
}
HAL_ADC_Stop(&hadc);
MCUTemperatureDegrees = __LL_ADC_CALC_TEMPERATURE(3300, ADCValue, LL_ADC_RESOLUTION_12B);
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Appreciate any help, I know I really should convert this to using DMA but I do not currently have time and this section is low-priority.
Kind Regards
#polling #adc #hal #stm32f0Solved! Go to Solution.
- Labels:
-
ADC
-
STM32Cube MCU Packages
-
STM32F0 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-11 7:02 AM
my ADC_init has these different lines...
hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; // = (0x00001000U) sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-11 2:43 AM
Hi
Botha.Antonie
,Try to have a look to this example under the STM32F0 firmware package, it may help you :
STM32Cube_FW_F0_V1.7.0\Projects\STM32F072B-Discovery\Examples\ADC\ADC_RegularConversion_Polling
This example describes how to use the ADC in Polling mode to convert data through the HAL API.
-Nesrine-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-11 4:52 AM
Hi
ELMHIRI.Syrine
‌,I have looked at that example,it unfortunately only uses one channel and thus Scan is set to Disabled. It also only gets the conversion once. I want to know how to use that mode to read multiple channels.
Kind Regards
Antonie
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-11 7:02 AM
my ADC_init has these different lines...
hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; // = (0x00001000U) sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-12 4:14 AM
Thank you
Marsh.Nick
‌, changing from'ADC_OVR_DATA_PRESERVED'to '
ADC_OVR_DATA_OVERWRITTEN' fixed my problem!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-23 2:50 AM
hi, why i get this error and warning?
error: use of undeclared identifier 'LL_ADC_RESOLUTION_12B'
warning: implicit declaration of function '__LL_ADC_CALC_TEMPERATURE'is invalid in C99- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-25 2:41 AM
Hi , your code is correct and must, Ranks 2,3, and 4 seems Rank 1, you should be use of Array for get a ADC Result same Below :
HAL_ADC_Start(&hadc);
uint16_t ADCValue[4] = 0x00;
uint16_t MCUTemperatureDegrees = 0;
if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) == HAL_OK)
{
ADCValue[0] = HAL_ADC_GetValue(&hadc); /* Gets CH1 */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue[1] = HAL_ADC_GetValue(&hadc); /* Gets 3V3 */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue[2] = HAL_ADC_GetValue(&hadc); /* Gets 5V */
HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);
ADCValue[3] = HAL_ADC_GetValue(&hadc); /* Gets Temp */
}
HAL_ADC_Stop(&hadc);
MCUTemperatureDegrees = __LL_ADC_CALC_TEMPERATURE(3300, ADCValue, LL_ADC_RESOLUTION_12B);