STM32CubeMX L4 V1.13.0 HAL_OSPIM_Config corrupts port configuration.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-09-09 12:20 AM
We are using STM32Cube_FW_L4_V1.13.0 and ran into trouble using two Octo SPI controllers with one running in Octo and one running in Quad mode.
While configuring the Quad mode IO ports with HAL_OSPIM_Config the configuration of the second one got corrupted. Had to patch the stm32l4xx_h
Labels:
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0