STM32CubeF0 compilation using arm-none-eabi-gcc and Makefile.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-28 1:39 AM
Posted on October 28, 2014 at 09:39
I'm trying to get a STM32Cube project compiled using arm-none-eabi-gcc and a Makefile. I have specified:
CFLAGS = -mthumb\
-march=armv6-m\
-mlittle-endian\
-mcpu=cortex-m0\
-ffunction-sections\
-fdata-sections\
-MMD\
-std=c99\
-Wall\
-g\
-D$(PART)\
-c
and:
LDFLAGS = -Wl,--gc-sections\
-Wl,-T$(LDFILE)\
-Wl,-v
The FW builds without problems.but when I boot the MCU i get stuck in Hard Fault. Stack trace is:
#0 HardFault_Handler () at ./Src/main.c:156
#1 <
signal
handler called>
#2 0x0800221c in ____libc_init_array_from_thumb ()
#3 0x080021be in LoopFillZerobss () at Src/startup_stm32f030x8.s:103
#4 0x080021be in LoopFillZerobss () at Src/startup_stm32f030x8.s:103
Backtrace stopped: previous frame identical to this frame (corrupt stack?)
and I go straight to Hard Fault when stepping to bl __libc_init_array in the startup file.
/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2]
adds r2, r2, #4
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the application's entry point.*/
bl main
Any ideas what could be wrong?
My arm-none-eabi-gcc version is 4.8.4 20140725 (release)
[edit] The disassembly of the calls
08002218 <
____libc_init_array_from_thumb
>:
8002218: 4778 bx pc
800221a: 46c0 nop ; (mov r8, r8)
800221c: eafff812 b 800026c <
__libc_init_array
>
0800026c <
__libc_init_array
>:
800026c: e92d4070 push {r4, r5, r6, lr}
8000270: e59f506c ldr r5, [pc, #108] ; 80002e4 <
__libc_init_array
+0x78>
8000274: e59f606c ldr r6, [pc, #108] ; 80002e8 <
__libc_init_array
+0x7c>
8000278: e0656006 rsb r6, r5, r6
800027c: e1b06146 asrs r6, r6, #2
8000280: 12455004 subne r5, r5, #4
8000284: 13a04000 movne r4, #0
8000288: 0a000005 beq 80002a4 <
__libc_init_array
+0x38>
800028c: e2844001 add r4, r4, #1
8000290: e5b53004 ldr r3, [r5, #4]!
8000294: e1a0e00f mov lr, pc
8000298: e12fff13 bx r3
800029c: e1560004 cmp r6, r4
80002a0: 1afffff9 bne 800028c <
__libc_init_array
+0x20>
80002a4: e59f5040 ldr r5, [pc, #64] ; 80002ec <
__libc_init_array
+0x80>
80002a8: e59f6040 ldr r6, [pc, #64] ; 80002f0 <
__libc_init_array
+0x84>
80002ac: e0656006 rsb r6, r5, r6
80002b0: eb0007ca bl 80021e0 <
_init
>
80002b4: e1b06146 asrs r6, r6, #2
80002b8: 12455004 subne r5, r5, #4
80002bc: 13a04000 movne r4, #0
80002c0: 0a000005 beq 80002dc <
__libc_init_array
+0x70>
80002c4: e2844001 add r4, r4, #1
80002c8: e5b53004 ldr r3, [r5, #4]!
80002cc: e1a0e00f mov lr, pc
80002d0: e12fff13 bx r3
80002d4: e1560004 cmp r6, r4
80002d8: 1afffff9 bne 80002c4 <
__libc_init_array
+0x58>
80002dc: e8bd4070 pop {r4, r5, r6, lr}
80002e0: e12fff1e bx lr
80002e4: 08002258 .word 0x08002258
80002e8: 08002258 .word 0x08002258
80002ec: 08002258 .word 0x08002258
80002f0: 08002260 .word 0x08002260
[edit 2] The register values from gdb:
(gdb) info reg
r0 0x20000000 536870912
r1 0x1 1
r2 0x0 0
r3 0x40021000 1073876992
r4 0xffffffff -1
r5 0xffffffff -1
r6 0xffffffff -1
r7 0x20001fd0 536879056
r8 0xffffffff -1
r9 0xffffffff -1
r10 0xffffffff -1
r11 0xffffffff -1
r12 0xffffffff -1
sp 0x20001fd0 0x20001fd0
lr 0xfffffff9 -7
pc 0x800067c 0x800067c <
HardFault_Handler
+4>
xPSR 0x61000003 1627389955
#gcc-arm-stm32-cortex-m-cubef0
Labels:
- Labels:
-
STM32Cube MCU Packages
-
STM32F0 Series
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-28 4:32 AM
Posted on October 28, 2014 at 12:32
Hi,
That __libc_init_array is ARM code, not Thumb, hence the M0 will fall over trying to execute some nonsense it doesn't understand (actually, it never quite gets there since it faults on the attempt to switch to ARM state in the bx, but hey, same difference...)You'll need to make sure you use pure-Thumb versions of any libraries - a Cortex-M-specific toolchain might be a better bet than a generic ARM one. If you have a multilib toolchain, I'd suggest checking the output of arm-none-eabi-gcc --print-multi-lib to make sure you've specified all the relevant options to get proper Cortex-M libraries, and if you're using a separate link step, make sure you invoke it with LD=arm-none-eabi-gcc (plus the relevant multilib options), rather than LD=arm-none-eabi-ld.PS: It seems you are missing to give -mcpu=cortex-m0 and -mthumb as link time flags.Regards,Heisenberg.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-30 9:57 AM
Posted on October 30, 2014 at 17:57
Thanks Heisenberg. It's ok for me !