cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C011 Clock Config

saraacri
Associate

Hi @ST Community ,

I struggle to configure the clock speed to the frequency I desire.

The chip I am using is STM32C011F6U and the code I use as first function in main() is the following:

uint16_t cr = RCC->CR;
uint16_t cal = RCC->ICSCR;
uint16_t cfgr = RCC->CFGR;

//Reset Clock divider to 1 (full 48MHz)
cr &= ~(RCC_CR_HSIDIV_0 | RCC_CR_HSIDIV_1 | RCC_CR_HSIDIV_2);
cr |= (1U << 11);
cr |= (1U << 12);
cr |= (1U << 13);
RCC->CR = cr;

//Enable HSI48 Clock
RCC->CR |= RCC_CR_HSION;

//Wait for HSI to be ready
while((RCC->CR &= RCC_CR_HSIRDY) == 0u);

//Default HSI calibration trimming value
cal &= ~RCC_ICSCR_HSITRIM;
cal |= RCC_ICSCR_HSITRIM_6;
RCC->ICSCR = cal;

//Set APB divider to 8
cfgr &= ~RCC_CFGR_PPRE;
cfgr |= (RCC_CFGR_PPRE_2 | RCC_CFGR_PPRE_1);
RCC->CFGR = cfgr;

//Set AHB divider to 1
cfgr &= ~RCC_CFGR_HPRE;
RCC->CFGR = cfgr;

 

However the above doesn't seem to have any effect and the clock frequency never change. I have also tried to output the SYSCLK using the MCO pins.

What am I doing wrong or missing?

Thanks!

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Super User

make a project with CubeMX , set clock tree as you want it, generate code -> and look there, what you should write

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Super User

make a project with CubeMX , set clock tree as you want it, generate code -> and look there, what you should write

If you feel a post has answered your question, please click "Accept as Solution".
EXUE.2
ST Employee

the normal clock configuration is as below in our example and CubeMX, you also can get the official example project in ST official website.

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
  {
    Error_Handler();
  }
}